EZ FX provides versatile, user-friendly and cost-effective camera jibs to the film and video production industries. The company carries two main products known as the EZ FX Jib and the While searching for an alternative solution over bronze bushings more than three years ago, EZ FX discovered igus Inc.’s line of iglide plain plastic bearings. The company now uses iglide G300 and iglide M250 on all of its jibs for a number of reasons. Designed to be economical, all-around bearings, the G300 and M250 enable EZ FX to reduce costs dramatically. Iglide G300’s ability to handle heavy loads also makes it a suitable match for the jib. Iglide G300 helps the camera, which can weigh up to 50 pounds, to pivot up and down in a seesaw motion with ease, while both bearings prevent corrosion between the aluminum rod of the jib and steel nuts and bolts. Steve Bonin, owner of EX FX, says iglide bearings are easy to work with. “We see many benefits from the iglide bearings. They reduce friction, are lighter weight than bronze and are cleaner to work with,” said Bonin. “They are also a major cost savings, which is great for us and our customers.” EZ FX provides its jibs to customers across the globe involved in a number of different productions. The jibs are used at television stations, churches, weddings and on the set of motion pictures, to name just a few. EZ FX is pleased with the benefits iglide has provided for the company and its customers. To learn more about EX FX, visit www.ezfx.com. |
|
Click to view |