Solutions for the manufacturing industry on display IMTS 2014 by plastics specialist igus9/2/2014

igus Inc., manufacturer of engineered plastic components for a wide range of industries, will be showcasing a variety of solutions for a multitude of applications at the upcoming IMTS 2014 trade show in booth 5677 in the East Hall of Chicago’s McCormick Place.

On display

At IMTS, igus will have on display a number of industrial solutions, including their e-spool and Triflex RSP Energy Chain Systems, DryLin E motorized linear systems, and heavy-duty PRT slewing ring bearings, all extensively tested in the igus test lab for reliability to lower customer maintenance and downtime.

Solutions for a variety of manufacturing challenges

The e-spool system connects two different energy supply systems in one system – a standard energy chain guided by a reel that always supports the proper length and tension of the energy supply system, and an igus TwisterBand that performs rotational movements. This design allows movements in any direction, making it suitable for a number of fields of application. For energy supply on robotic systems, igus is offering the Triflex RSP, which supplies continuous adjustable retraction force for the Triflex multi-axis cable carrier system. Using maintenance-free, self-lubricating linear guides, the RSP system is a slim, open system which allows for both lightweight, open-style chains, or heavy-duty closed styles.

Also on display will be the new DryLin E, or ‘Electric’, system, a ready-to-install linear axis with motor. A lightweight design with choice of belt or lead screw drive, and a variety of motors, this new system is custom-built and shipped in 3-4 days in 15 variations.

igus’ polymer slewing ring bearings, which use self-lubricating, low-friction sliding elements in place of ball bearings, will also be out for demonstration at IMTS. Available with a variety of options, like gears and optional stainless steel versions, they are light weight and low cost, yet rugged and durable enough for even the toughest rotary applications.

To schedule a visit with an igus representative at the show, or to learn more about IMTS, please visit www.igus.com/Fairs.


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302