Home > Press Room > Photo Gallery
Photo Gallery
Energy Chain Systems ReadyChain Chainflex iglide, DryLin & igubal igus Company
View the igus gallery and choose any photograph and caption for print or online publication. These photos are for media only and should not be used for any other purposes. Please contact Courtney Toomey with questions or comments or to let us know of an impending publication at ctoomey@igus.com or call (800) 521-2747.

 
Energy Chain Systems®
SWS uses Energy Chain

Hi-Res/Lo-Res Hi-Res/Lo-Res Hi-Res/Lo-Res
The Shanghai Waigaogiao Shipbuilding Company (SWS) uses igus® cable management systems on three of its ship-to-shore cranes.
E-Z Chain Carriers Enable Easy Cable Access

Hi-Res/Lo-Res
The E-Z Chain split crossbars are flexible, but retain their shape and strength to provide secure protection and easy cable accessibility. This is achieved through a unique crossbar design, which consists of two, memory-retaining plastic pieces.
Cable Carriers for Six-Axis Robots

Hi-Res/Lo-Res

The Triflex RS System is well suited for welding applications in tight areas, multiple-tool applications, material handling jobs and deburring applications.

Guide Troughs help E-Chain Move Smoothly

Hi-Res/Lo-Res Hi-Res/Lo-Res
Guide troughs are available through igus as separate components or fully assembled systems. They also can come equipped with glide bars, which are installed in the trough for the Energy Chain or tube to glide along. Glide bars are made of abrasion-resistant polymer and virtually eliminate noise and friction.
Triflex uses Improved Fiber Rod

Hi-Res/Lo-Res Hi-Res/Lo-Res Hi-Res/Lo-Res
After many series of tests, igus has implemented an iglide® bearing on the moving tips of its fiber rods to increase the torsional strength and better cope with the extreme, twisting movements often demanded in robotic applications at the touch of a button.
Barco uses Energy Chain and Chainflex

Hi Res/Low Res  Hi Res/Low Res
Barco Media uses System E4 to house and protect vital Chainflex cables on an outdoor, larger-than-life, eight-screen LED display located at Victory Plaza in Dallas, Texas.
Chainflex and E-Chain in cleanrooms

Hi Res/Low Res  Hi Res/Low Res
Igus now offers both control and servo cables for near-sterile environments, as well as ISO-approved cable carriers within the families of System E3, System E4/100, System E6 and E-Z Chain.
"Zipper" Energy Chains

Hi Res/Low Res Hi Res/Low Res
“Zipper” Energy Chains make cable installation and removal—especially for cables equipped with preassembled connectors—both fast and simple.
System E4/4 Energy Chain

Hi Res/Low Res
The System E4/4 Energy Chain® line was developed for heavy-duty and demanding applications in harsh environments, making it an ideal solution for cranes used in port machinery, material handling and other indoor/outdoor applications.
System E6 Energy Chain

Hi Res/Low Res
System E6 is uniquely designed with abrasion-resistant connector strips—rather than a pin and bore configuration—that when combined with a short link pitch produces little to no noise even at high speeds.
The quicksnap accessory

Hi Res/Low Res
Quicksnap is ideal for applications requiring frequent cable replacement or applications where a single power source is used on multiple machines.
Triflex R for robots

Hi Res/Low Res
Triflex R protects moving cables and hoses, including igus’ line of Chainflex® continuous-flex cables, attached to automated robotic machinery.
AUTO-GLIDE family

Hi Res/Low Res
AUTO-GLIDE system enables Energy Chain cable carriers to glide on themselves in long travel applications without guide troughs.

Improved AUTO-GLIDE with floor bumpers and positioning guide

Hi Res/Low Res  Hi Res/Low Res

Improved AUTO-GLIDE System now with floor bumpers and positioning guides for further retention of alignment.
Crossbars

Hi Res/Low Res
Polymer crossbars outperform aluminum crossbars in stress and wear tests.
System E2 Energy Tubes

Hi Res/Low Res
System E2 Energy Tubes fully protect cables from debris while providing fast, easy access with snap-open hinges.
System E3

Hi Res/Low Res
E3 Energy Chain cable carriers: a low-cost low-noise solution
System E4/100 Energy Chains easily support 750 pounds of weight and withstands the most demanding applications.
Energy Chain catalog

Hi Res/Low Res
Energy Chain Systems catalog is chock-full of design and engineering data, application examples and all the tools to specify the right cable carrier for any application.
Energy Tube

Hi Res/Low Res
Energy Tube enclosed Energy Chains shield cables from debris and contaminants such as dirt, wood chips, metal filings, spatter, hot chips, dirt, dust, cooling agents and various chemicals.
ESD Energy Chains

Hi Res/Low Res
ESD Energy Chains are critical for for applications with hazardous or potentially explosive conditions.
Extender crossbars

Hi Res/Low Res

Extend the possibilities with extender crossbars from igus.

E-Z Chain

Hi Res/Low Res
Perform fast, simple cable installation with E-Z Chain from igus.
E-Z Triflex
 
Hi Res/Low Res
E-Z Triflex cable carriers deliver multi-axis movement for robotic applications and tight space restrictions. By adding the ease of installation enjoyed with the E-Z Chain design, customers can add and remove cables in a snap.
Interior separators

Hi Res/Low Res

Igus Energy Chains employ modular separation of cables and hoses to safely deliver data and power to automated systems.

Machine tool debris

Hi Res/Low Res
Igus Energy Tubes are designed to withstand a barrage of harsh conditions, including extreme weather, debris such as metal filings and wood chips, and other foreign objects.
Micro chains

Hi Res/Low Res
Micro chains are ideal for tight space restrictions and small bending radii, proving good things do come in small packages.

Rol-E-Chain

Hi Res/Low Res

Rol-E-Chain cable carriers: an innovative and breakthrough design based on one of the simplest mechanical elements--the wheel.
SnapChain

Hi Res/Low Res
Energy Chain SnapChain with adjustable loops facilitates cable bundling.
New Triflex R sports a smooth tubular design for seamless movement and a trailer-hitch style construction for strength and flexibility.
Case IH uses E2 Energy Chain

Hi Res/Low Res
Case IH, a worldwide leader in the farm equipment industry, has been using System E2 Energy Chain® to house and protect hydraulic cables on its line of 1200 ASM Series Planters.
High temperature E-Chain

Hi Res/Low Res
The fully enclosed Energy Tube is constructed with igumid HT, a pioneering polymer material that is unaffected by hot chips reaching temperatures of 1,500 degrees Fahrenheit and higher.
System E1 Energy Chain

Hi Res/Low Res
System E1 Energy Chain, a cost-effective cable carrier with an easy-to-open, multilink band, is designed to be a simple solution for smaller, less complex, cable-management requirements.
Speed-E-Chain

Hi Res/Low Res Hi Res/Low Res
New micro Speed-E-Chain is a space-saving, compact system for rack control devices that operates safely and silently at high speeds.

 

ReadyChain Systems
2007

PMT uses ReadyChain

Hi-Res/Lo-Res Hi-Res/Lo-Res
Portsmouth Marine Terminal (PMT), operated and maintained by Virginia International Terminals (VIT), uses ReadyChain—igus’ complete, preassembled cable carrier systems that combine Energy Chain® cable carriers with the company’s Chainflex cables.
Out-of-the-box simplicity

Hi Res/Low Res
igus ReadyChains are a simple, easy-to-install, complete Energy Chain System available straight from the box and onto your machine.
ReadyChain harnessing service

Hi Res/Low Res
ReadyChains are pre-assembled cable carriers, complete with cables, carrier, strain relief, connectors and any other accessories. Enjoy one-stop shopping.
Price Industries ReadyChain on a spool

Hi Res/Low Res
Igus ReadyChains used by Price Industries on its high speed cranes lower costs and increase production throughput for this leading OEM.
Price ReadyChain installed at SuperSteel

Hi Res/Low Res
Price crane with ReadyChain installed at Super Steel Treating Company.

 

Chainflex® continuous-flex cables
2007

Continuous-Flex Cables for USB Applications

Hi-Res/Lo-Res

With an overall shield for increased EMI protection, Chainflex USB cables are unaffected by high-noise, industrial environments where crosstalk can be a problem. They are also silicon-free according to PV 3.10.7 and are UL AWM, ROHS and CE compliant.

Industrial FireWire Cables

Hi-Res/Lo-Res
Industrial standard FireWire cables typically fail prematurely over long distances because they are not designed with constant flexing in mind. igus has solved this problem with a combination of its specially constructed Chainflex® CFBUS.055 FireWire cable and its Energy Chain® cable carriers
Flame-Resistant Control Cables

Hi-Res/Lo-Res
The new UL- and CSA-approved versions have a bending radius of 5xd and a flame-resistant TPE outer sheath. The cables also remain highly flexible even when exposed to extreme temperatures ranging from -31 to +212 degrees Fahrenheit.
CF21 and CF27 high-flex servo cables

Hi Res/Low Res
Hi Res/Low Res
Supported by tests, not just theory, CF21 and CF27 perform through millions of cycles in short or long travel applications, even with a small bend radius of 7.5 times the outer cable diameter.
Chainflex CF7 and CF8

Hi Res/Low Res
CF7 and CF8 are equipped with short-pitch conductor twisting for long cable life and are ideal for demanding, high-flex applications.
Chainflex CF9 and CF10

Hi Res/Low Res
CF9 and CF10 are two of the most resistant cables to emerge from the bunch, as they are equipped with bare copper conductors and are fully resistant to oil, frost, chemicals and exceptionally low or high temperatures.
Chainflex CFBUS

Hi Res/Low Res
The CFBUS series supports Profibus, DeviceNet, Interbus, Can-Bus, Firewire, USB and Ethernet industrial networks. These special cables are designed to flex for millions of cycles and provide fast, reliable data transmission.
Chainflex star-quad design

Hi Res/Low Res
These Chainflex cables can replace standard twisted-pair cables in most applications. When EMI-dampening and signal clarity are critical to an application, such as in the electronic, medical and entertainment industries, this type of cable configuration is especially beneficial.
CAT 5/ethernet data cables

Hi Res/Low Res
Chainflex Category 5 Ethernet cables are designed for high speed data transmission systems and transmit up to 100 Megabits per second.
Chainflex Air pneumatic hoses

Hi Res/Low Res
Chainflex Air hoses have been successfully tested for more than 10 million cycles at a bend radius 10 times the outer diameter while installed in an E-Chain.
CF130 & CF140

Hi Res/Low Res
Chainflex CF130 & 140 cables are an affordable continuous-flex tray cable for control and power systems.
CF211 & CF240

Hi Res/Low Res
Chainflex cables deliver cost-effective data transmission solutions.
CF300

Hi Res/Low Res
Crank it up with Chainflex CF300 high-voltage, high-amperage flexible power cable.

CF98

Hi Res/Low Res
Hi Res/Low Res

Chainflex CF98 squeezes its way into ATM machines and high-speed pick-and-place robotic applications with its unique copper alloy and a bend radius of just four times the outer diameter—the smallest to date.
CF170

Hi Res/Low Res
Chainflex CF170 from igus: low-cost cable for machine tools.
Designed for ECS

Hi Res/Low Res
Chainflex continuous-flex cables from igus are designed specifically for use in an Energy Chain System for a complete, safe and long-lasting energy supply system.
General Chainflex

Hi Res/Low Res
Hi Res/Low Res
Igus Chainflex continuous-flex cables cables withstand the stress of tight bending radii and deliver longer extended life at a lower cost.
Skydrol resistant

Hi Res/Low Res
Fly away with Chainflex cables with thermoplastic elastomer (TPE) jackets that are completely resistant to Skydrol®, the aircraft industry’s leading phosphate-ester hydraulic fluid.
Strain Relief

Hi Res/Low Res
Chainflex tie wraps and plates ensure the security of Energy Chain cable management systems.

Allen Bradley

Hi Res/Low Res

Igus offers a line of continuous-flex, drive, interconnect cables especially for Allen Bradley “MP series” industrial automation systems.
Chainflex CFLG

Hi Res/Low Res
Chainflex CFLG combines the high optical transmission quality of glass with the ability to deliver a superior performance, even in harnessed, high-flex applications.
Chainflex CF.INI

Hi Res/Low Res
Chainflex CF.INI can withstand severe weather conditions with an approved temperature range of -31 to +212 degrees Fahrenheit.

 

iglide® plastic bearings, DryLin® linear bearings, igubal® spherical bearings

igus Exhibits at Western Canada Farm Progress Show

Hi-Res/Lo-Res Hi-Res/Lo-Res
igus will be displaying its iglide® plain bearings, which are dirt- and fertilizer-resistant, low cost and can cope with up to 21,750 pounds per square inch (PSI).
Long-Life Bearings Better for Environment

Hi-Res/Lo-Res Hi-Res/Lo-Res
igus® Inc. will be exhibiting at NeoCon from June 9-11. The company will be primarily promoting its self-lubricating polymer plain bearings for office chair pivot points at the show.
Bearings for the Boating Industry

Hi-Res/Lo-Res Hi-Res/Lo-Res Hi-Res/Lo-Res
igus® Inc. today announced that Quality Boat Lifts uses iglide® plastic, plain bearings on its lifts used by both residential and commercial marinas and private owners to remove boats from the water.
Bearings offer Environmental Benefits

Hi-Res/Lo-Res
Due to continually advancing bearing technology, igus is able to supply metal plain and rolling bearing alternatives more in line with environmental considerations for an increasing number of applications.
DeepRock uses DryLin

Hi-Res/Lo-Res Hi-Res/Lo-Res Hi-Res/Lo-Res
The company chose DryLin R bearings because they are impervious to the various outdoor elements encountered by its drilling machines. Previously, dirt and mud constantly dropping onto the components and creating sludge caused the rack-and-pinion system to fail.
Polymers now Machinable

Hi-Res/Lo-Res Hi-Res/Lo-Res
The 2-inch diameter solid rod is available in either iglide R or iglide J: two high quality bearing materials not accessible anywhere else on the market as semi-finished products.
Self-Lubricating Slewing Rings

Hi-Res/Lo-Res
iglide PRT slewing ring bearings are suitable for all environments; in particular, semiconductor and cleanroom applications, assembly lines, production facilities and robots.
DryLin Easy Tube

Hi-Res/Lo-Res

DryLin EasyTube is a completely lubrication-free, compact and lightweight system, consisting of just six individual parts: a leadscrew, tube, two clamping rings, an attachment flange and slide block.

Mini Bearings are Light, Resilient

Hi-Res/Lo-Res
The mini plain bearing is part of igus’ line of igubal® spherical bearings. It requires minimal installation space and can be supplied immediately ex-stock. The self-aligning bearing is light and compact, requires no lubrication, is simple to install and adapts to all angular misalignments.
e-Ride Industries uses igubal

Hi Res/Low Res Hi Res/Low Res
e-Ride Industries uses igubal pillow blocks and clip bearings on the steering shafts and suspensions of its electric utility vehicles.
DryLin W

Hi Res/Low Res
Stainless steel DryLin W is ideal for harsh environments such as underwater, chemical and wash down, or for applications ranging from packaging to food and beverage, textile and marine.
igubal clip bearings

Hi Res/Low Res
Igubal clip bearings eliminate the misalignment issues often encountered when using imprecisely formed sheet metal and are ideal for both office equipment and automotive seating applications, to name a few.
iglide J

Hi Res/Low Res
Iglide J is ideal for both high-speed and low-speed applications, as it operates flawlessly at rates up to 1,968 feet per minute (fpm) in linear motion and 197 fpm in rotary motion.
iglide medical brochure

Hi Res/Low Res
The easy-to-use, 10-page brochure includes a rundown of the features and benefits of such iglide bearings as iglide R, a low-cost replacement for bronze bearings; iglide T500, a high-temperature bearing with superior chemical resistance; and iglide A200, ideal for applications requiring FDA-approved material.
iglide T500 series

Hi Res/Low Res
Iglide T500 is an ideal choice for both oscillating, high-loads and high-frequency, low-load applications. In applications with low speeds and radial pressures higher than 8,700 psi iglide T500 lasts twice as long as coated or lubricated metal bearings.
Custom iglide

Hi Res/Low Res
Igus will custom-mold any of its iglide polymer materials to fit the size and shape of any machine.
DryLin N17

Hi Res/Low Res
DryLin N17 is the smallest linear guide system available from igus.
DryLin R

Hi Res/Low Res
If you have a need for speed and low-noise, DryLin R linear bearings are the choice for you.
DryLin R and DryLin S never rusts

Hi Res/Low Res
Rest easy, the DryLin R and DryLin S power-packed combo eliminates rust and contamination for a worry-free solution.
DryLin S shafting

Hi Res/Low Res
Lighten the load with DryLin S lightweight aluminum shafting.
DryLin spindle-lift tables

Hi Res/Low Res
New plastic spindle-lift table is lightweight and low-cost while its sister super-flat spindle lift fits into the smallest space restrictions.
DryLin W

Hi Res/Low Res Hi Res/Low Res
New DryLin W is a compact, versatile, easy to install solution available in multiple rail configurations for unlimited design options.
DryLin WQ

Hi Res/Low Res
DryLin WQ square rails reduce friction and can be adapted to float and realign to accommodate varying heights along the plane.
General iglide

Hi Res/Low Res
Iglide plastic bearings from igus are a self-lubricating, maintenance-free and contamination-free replacement for traditional metal bearings.
iglide for automotive applications

Hi Res/Low Res
Iglide goes along for the ride in a multitude of automotive applications.
iglide G300

Hi Res/Low Res
Iglide G300 sustains performance in rugged off-highway applications.
iglide H370

Hi Res/Low Res
Iglide H370 plastic bearings from igus are water-resistant.
iglide R

Hi Res/Low Res
Look no further, iglide R is the ideal replacement for bronze bearings at a lower cost and with a longer life.
igubal clevis joint

Hi Res/Low Res
Igubal all-plastic clevis joints make the connection.
igubal spherical bearings

Hi Res/Low Res
Igubal spherical bearings round out the complete bearing selection from igus.

iglide J

Hi Res/Low Res

Iglide J polymer blend is used throughout igus' extensive line of motion control solutions, from plain bearings to linear guide systems.
Catrike tricycle uses igubal

Hi Res/Low Res
Igubal spherical bearings provide smooth steering for recumbent tricycle enthusiasts.
DryLin T for woodworking

Hi Res/Low Res
DryLin T linear guide system impervious to wood chips and sawdust making it a clear choice for the woodworking industry.
DryLin linear bearings

Hi Res/Low Res
DryLin linear bearings and guide systems are wear-resistant, self-lubricating, contamination and corrosion-free and have a low coefficient of friction.
DryLin ZLW

Hi Res/Low Res
DryLin ZLW is ideal for quickly positioning small loads and can be employed in a number of industries from packaging to medical technology to food and beverage.
Rogers Sprayers

Hi Res/Low Res
Rogers Sprayers offers two types of boom sprayers—the Windfoil™ and the Falcon™—which both use as many as 30 iglide R and iglide J bearings at various pivot points to prevent metal-on-metal contact.

 

igus® Company

igus to Show at IWF

Hi-Res/Lo-Res
The company will be promoting its Energy Tubes at the show, which are fully enclosed cable carriers designed to protect cables and hoses from falling woodchips and debris.
igus to Exhibit at ATX East

Hi-Res/Lo-Res
igus® has announced it will be exhibiting at this year’s Automation Technology Expo from June 3-5 at the Jacob K. Javits Convention Center in New York.
igus to Exhibit at Del Mar Show

Hi-Res/Lo-Res
igus® Inc., will be promoting its cable carriers, continuous-flex cables, self-lubricating bearings and lubrication-free linear guides on booth #261 at the forthcoming Del Mar Electronics Show (DMES).
2D and 3D CAD Files from igus

Hi-Res/Lo-Res Hi-Res/Lo-Res
Visitors to the company’s website—www.igus.com—can access CAD files for each of igus’ comprehensive lines of Energy Chain® cable carriers, iglide® plastic plain bearings, igubal® spherical bearings and DryLin® linear bearings and guide systems.
FIRST Teams in "Overdrive"

Hi-Res/Lo-Res
All 1,500 participating FIRST teams have the opportunity to use various plastic machinery components donated by igus® Inc., the leading developer of Energy Chain Systems®, Chainflex® continuous-flex cables and iglide® plastic bearings.
Iowa State University

Hi-Res/Lo-Res Hi-Res/Lo-Res
Students from Iowa State University used igubal® spherical bearings, DryLin® R linear bearings and DryLin linear guide systems to develop a basketball shooter. The device enables children with Cerebral Palsy to participate in basketball games with friends.
igus CD Catalog

Hi Res/Low Res
BEST Robotics teams used donated igus plastic machinery components for the third consecutive year.
igus CD Catalog

Hi Res/Low Res
This first-ever, fully searchable CD-Rom provides the complete product and design information contained in the company’s acclaimed print catalogs.
Sussex County Tech High School

Hi Res/Low Res
The Sussex County Tech team used both DryLin T linear guide systems and igubal flange bearings, donated free of charge by igus in conjunction with its Y.E.S. Program.
University of Buffalo

Hi Res/Low Res
Students studying architecture at the University of Buffalo used donated igubal spherical bearings and DryLin S aluminum shafting on a unique project. The team built a device capable of hiding a person.
Texas A&M Students

Hi Res/Low Res Hi Res/Low Res
Students from the University of Texas A&M show off an igus Energy Chain System that they used to test the effects of acceleration on spatial orientation of liquid and ullage. The students performed the experiment aboard NASA's Weightless Wonder.
URI Mini Baja vehicle

Hi Res/Low Res
Igus is a proud sponsor of the University of Rhode Island Mini Baja team. The 2003-2004 team used an igubal spherical bearing to support the steering shaft on its off-road vehicle.
Student product donation

Hi Res/Low Res
Igus donated DryLin W to students at Harker High School in California. The students plan to use DryLin W to create a telescoping elevator on the FIRST 2005 robot entry.
igus offers free samples

Hi Res/Low Res
Igus offers a complete array of samples for any product so customers can find the right solution for their application.
New Quebec sales office

Hi Res/Low Res
Igus appoints new regional manager of Quebec sales office, Steve Gougeon.

Cornell University Racecar

Hi Res/Low Res

Students from Cornell University used igubal® spherical bearings on the steering assembly of their 2005 Formula SAE (Society of Automotive Engineers) racecar.
igus Donates to FIRST

Hi Res/Low Res Hi Res/Low Res
Igus announced it would donate Energy Chain, iglide, and DryLin as well as igubal spherical bearings to more than 1,130 teams that hail from the U.S. and 6 other nations, including Brazil, Canada, Ecuador, Israel, Mexico and the United Kingdom.
Upper Darby High uses igus

Hi Res/Low Res Hi Res/Low Res
In conjunction with the company’s Y.E.S. Program, designed to foster the mechanical design ideas of students with a passion for engineering, igus provided the Upper Darby team with plastic machinery components.
igus helps Grady High School with Laundry Quandry

Hi Res/Low Res
Grady High used a DryLin N linear guide system on its robot's scissor-lift device. Igubal spherical bearings were used at the pivot points of both the main drive wheel and caster wheels because of their durability and low friction.

webmaster@igus.com
Copyright© igus Inc. All rights reserved.

igus® Inc. T: (800) 521-2747 F: (401) 438-7270 e-Mail: sales@igus.com