igus Demonstrating self-lubricating bearings and high-strength plastics for outdoor equipment at GIE+Expo10/17/2014

igus, manufacturer of self-lubricating plastic bearings, will be demonstrating the power of their plastic components at GIE+Expo 2014, the largest industry trade show for outdoor power equipment, lawn and garden equipment, and light construction and landscaping equipment. On display will be a selection of igus’ most reliable bearing materials for these types of applications, along with their igubal spherical rod-end bearings.

igubal rod end bearings handle high loads at normal room temperatures, have excellent dampening properties and weigh only a fifth of traditional metallic bearing rod end bearings, making them an excellent replacement for standard metal options. The resistance of igubal bearings to dirt and dust makes them ideal for applications where a standard greased bearing would not be suitable, such as in outdoor and agricultural applications.

Also on display will be igus’ line of self-lubricating plain bearings, iglide, which are currently celebrating 30 years of innovation. Swapping bronze bearings for iglide specialist plastics can increase service life in tough applications by 600% or more, while reducing costs by up to 80%. All iglide bearings are completely self-lubricating, so they will not attract dirt and debris which can cause bearings to seize. Additionally, liquids like water and chemicals will not affect bearing performance. For these reasons, among others, iglide plastic materials are a perfect solution for outdoor applications. To make an appointment with an igus representative at GIE+Expo, or to request a free entry pass, visit the igus tradeshow page at http://www.igus.com/Fairs.


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302