Submit Your Story

Product Demo Videos

News Room

Corner Home

igus Home

Click to view
larger image

 

 

 

 

Matrix Packaging Machinery prides itself on delivering rugged, well-engineered, cost competitive and easy-to-use packaging systems to customers around the globe. The company manufacturers vertical, form, fill and seal (v/f/f/s) packaging equipment, which handles a wide range of products from green beans to candy to detergent.

One of Matrix’ main product lines is its G Series—a group of packaging machines that includes the Matrix Proteus, Mercury and Ares. Because these machines operate in many diverse environments, Matrix needed a bearing that would operate seamlessly, while in continuous contact with environmental elements such as dust, dirt and water. The choice became clear when Matrix discovered igus®’ line of DryLin® R linear bearings, made of highly engineered plastic so they need no lubrication or maintenance. DryLin R bearings are formulated for long-life and consistently low friction.

Matrix uses DryLin R sleeve bearings designed for easy installation and removal in the most extreme applications, such as those seen by Matrix packaging machines. The bearing is comprised of two parts: a plastic liner made from igus’ iglide J material that can be pushed easily onto the shaft and a split aluminum adapter that fits over the liner.

This particular bearing delivers many advantages for both Matrix and its customers. Installation time is greatly reduced because Drylin R eliminates the need to remove the shaft from its housing. And if replacement is necessary, the adapter shell opens effortlessly and only the plastic liner needs to be replaced. This feature also saves the customer time, and in some cases, can reduce replacement part costs by 90 percent.

However, with DryLin R, Matrix customers rarely experience bearing failure on their machines. The company’s expectations were exceeded when DryLin R endured seven million cycles on its G Series with little to no noticeable wear, and to date, some of the machines have surpassed the 10-million cycle mark with DryLin R still in operation.

“Our products are sold all over the world and every machine operates in a different environment,” said Marcel Willden, president of Matrix. “Dusty or washdown environments, as well as a variety of other harsh conditions, are not unheard for our machines. With DryLin R, our customers do not have to worry about lubricating the bearings. Instead, they benefit from machines that run longer without service. DryLin R bearings are a low-cost, maintenance-free alternative to other solutions we have used.”

In the past, Matrix employed metal ball bearings in its packaging machines. After encountering scored shafting and grease leaks on some machines, Matrix made the switch to DryLin R. After doing so, the company has noticed little to no shaft wear and a slight increase in production due to the lighter weight of DryLin.

Matrix uses DryLin R linear bearings on its G Series machines, which are capable of reaching up to 160 cycles per minute. DryLin R manages loads up to 15 pounds on each machine, while operating at a speed of 750 feet per minute. Matrix’ machines also use iglide® Z from igus, a line of plastic bearings suited for applications with high temperatures, extreme loads and high surface speeds. To learn more about Matrix and its products, visit www.matrixpm.com.

For more information on DryLin R bearings, download the PDF file or fill out an information request form. You can also e-mail us at sales@igus.com, or call us: 888-803-1895.

 

 
webmaster@igus.com
Copyright© igus inc. All rights reserved.
 
igus® Inc. T: (800) 521-2747 F: (401) 438-7270 e-mail: sales@igus.com