|
||||
|
||||
Installment 1: Caring for Cables
|
||||
Any application involving moving machinery and constant repetitive motion will benefit from a cable carrier system. Typical applications range from machine tools, woodworking machinery and palletizers, to automated robots, cleanrooms and ship-to-shore cranes. igus'® line of cable carriers -- known as Energy Chains® -- are all-plastic, maintenance-free, corrosion-resistant cable carriers. They can replace metal or steel carriers in almost any application. igus offers a variety of Energy Chains such as: micro chains for the smallest applications, E-Z chain for quick assembly, E6 chains for low noise and low vibration, fully enclosed Energy Tubes for applications with flying debris and multi-axis cable carriers for robotic applications. |
||||
Types of installation The cable carrier is an integral part of any machine design and should be considered early-on in the design process. It can be implemented in a variety of ways depending on the motion of the machine, but the most common is a horizontal, unsupported, short-travel installation. In this type of application, the upper run of the carrier operates without touching the lower run throughout the entire length of travel. The maximum unsupported length is different for every application, but this type of configuration will have the longest service life (see image A). Image A
Image B |
||||
|
|
||||
Material selection Plastic cable carriers weigh much less than metal or steel alternatives, which reduces the power necessary to move the carrier and can help eliminate complex support systems. Plastic is also corrosion-free, quieter than metal, non-conductive and requires no lubrication. Many plastic carrier systems snap together without the use of metal fasteners which can easily shake loose and become embedded in the jacket of a cable or hose, or get jammed inside the carrier, impeding movement. Plastic carriers from igus® can be used in place of steel chains in a wide array of harsh environments. The only exception is applications with long term temperatures exceeding 266 degrees Fahrenheit. |
||||
9 Steps for specifying a cable carrier system Here is a step-by-step guide to specifying a cable carrier. 1. Gather data The first step in choosing a cable carrier is to gather all the necessary technical data prior to contacting a cable carrier vendor. This includes:
2. The largest cable or hose The first question any reputable cable carrier manufacturer will ask is, “What is the largest cable or hose in your system?” This will determine the minimum size of the cable carrier. To this number, add proper clearance—10% for cables and 20% for hoses—and the resulting dimension is the minimum inner height of the carrier. 3. Style, style, style Next, choose the style of carrier. Always choose a snap-open version whenever possible (see image C). This type of carrier allows access to cables with crossbars that snap open at any point along the carrier. Image C If debris or other external conditions are an issue, the tube-style cable carrier replaces the crossbars with lids to fully enclose the carrier and provide complete cable protection (see image D). This style is especially useful in applications where woodchips, metal filings and other debris are present. Image D igus® has pioneered various methods of cable access, such as split crossbars, “zippers” or hinged crossbars. With a split crossbar, simply press the conduit into the carrier to install and pull straight up to remove. For zipper-like removal of crossbars, the carrier has interconnected lids that are pulled back like a zipper, removing the top section of the carrier. The hinged crossbars are attached to the side links and are made of non-fiber, reinforced nylon to enable the hinge to flex. These designs minimize assembly and disassembly time (image E, F and G). Image E, F and G There also are modular cable carriers for heavy-duty, longer-travel applications. They are available with hinged crossbars that are opened on either the inner or outer radius, depending on which is preferable for the application, or with lids to make them into a tube for debris protection. Special cable carriers are available to meet a variety of application requirements. Some are:
It is important to analyze every aspect of your application in order to choose the right cable carrier. 4. The environment The environmental conditions of an application typically determine which type or style of carrier to use. If debris such as woodchips or metal shards are present, or if the application is in a dirty or contaminated area, an enclosed tube is ideal. An open crossbar carrier is lightweight and facilitates easy inspection and replacement of cables,whereas tube carriers offer removable lids for cable access. Also consider whether the application is underwater or comes in contact with liquids. igus® cable carriers will not corrode and are resistant to chemicals. Note: Space restrictions 5. Bend Radius All cable carriers have a predetermined radius stopping point on each link. When a number of links are assembled, these stopping points restrict the carrier from fully pivoting and form a curve loop or minimum bend radius. All cable carriers have multiple bend radii to choose from and all manufacturers suggest a minimum bend radius. If this is unknown, the general rule is 8-10 times the outer diameter of the largest cable or hose. The larger the bend radius, the less stress is placed on the cable and the longer the service life will be. Bend radius is measured from the center of the curve loop to the center of the pivot pin on the side link. Do not confuse this with the dimension of the overall curve height. Image H
Important Installation Dimensions The bend radius of the carrier is relative to the permissible bend radii of the cables and hoses. The ultimate function of a cable carrier is to ensure the cables and hoses bend properly and do not exceed the maximum bend radius. A cable carrier is only as flexible as its most inflexible conduit. 6. Cable and hose packages Since the primary function of a cable carrier system is to ensure proper bending of cables, it is imperative to install the conduits properly. To ensure maximum cycle life for your machine, the easiest solution is to use cables designed for use in a cable carrier. Chainflex® continuous-flex cables are designed specifically for use in Energy Chains®. Chainflex® cables follow these seven guidelines:
Image I
Rules of Distribution
The distribution rules are necessary because cables and hoses must be able to move freely at all times and tensile force must be prevented at the radius of the cable carrier. In high-speed applications and high cycles, cables cannot be laid on top of each other without horizontal separation. For travel speeds more than 1.64 ft/s (0.5 m/s) and cycles higher than 10,000 p.a., interior separators should be used. Follow these guidelines when designing the cable package:
There are, of course, exceptions to every rule. Therefore, it is highly recommended to speak with an igus® design technician to ensure your system will operate properly, with maximum lifespan. 7. Cable carrier length To determine how long a cable carrier your application will require, first determine the position of the fixed end. The ideal and most cost-effective position is at the center of travel. This will require the minimum amount of carrier to achieve the necessary movement. Use the following formula to determine the necessary cable carrier length: S = Maximum machine travel distance Use this formula if the fixed end is anything other than the center of travel: 8. Acceleration and inertia It is critical to ensure that the cable carrier is strong enough to support the application. If it isn’t, the results can be devastating. The carrier can literally snap in two. In order to ascertain that the carrier is strong enough, use the following formula to determine the force required for your application. First, determine the acceleration force. Acceleration force is the force required to keep the cable carrier moving once it has started. Acceleration Force (lb) = Total Weight lb (carrier and fill) x Acceleration ft/sec 2 Then determine the push force. Push force is the force required to get the cable carrier moving and overcome inertia. Once those numbers are determined, calculate the force of the application by: The force required must be less than the maximum force for the selected carrier. Cable carrier manufacturers typically do not publish the maximum force allowance for their products, but igus® technicians will calculate the force required for your application and select the proper size carrier to meet this requirement. 9. Accessories A variety of accessories are designed to further facilitate the energy supply system. They can include:
Strain relief is another common accessory designed to keep cables in position at both ends of the carrier. Sometimes strain relief at just the moving end is sufficient, depending on the application, and hydraulic or other fluid hoses should only be strain relieved on the moving end. Strain relief can consist of profile rails, clamps, tie wraps and tie wrap plates. Improper, or lack of, strain relief is a common cause of cable and hose failure. The strain relief clamps hold the cable in the neutral axis of the carrier. This prevents the cables from being pulled against the inner radius of the carrier or pushed against the outer radius of the carrier where it can be damaged or incur wear. While it may seem like an insignificant point, strain relief can often make—or break—the success of an application. Contact igus® for assistance in specifying a cable carrier for your application today by calling 1-800-521-2747 or e-mailing sales@igus.com. Or, click here to let igus specify the right Energy Chain System® for your application today! |
||||
| Back to Top | ||||
| Back to Tech Talk Home | ||||
webmaster@igus.com
Copyright© igus inc. All rights reserved. |
||||
igus® Inc. T: (800) 521-2747 F: (401) 438-7270 e-Mail: sales@igus.com |
||||