Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270
US(EN)

Safe, flexible cable guidance for KUKA articulated arm robots in aircraft construction

Airbus subsidiary uses triflex R and E4/4 plastic energy chains on axes 1 to 7

A KUKA robot suspended from the ceiling for aircraft component construction was to be equipped with various cable guidance systems on axes 1 to 7. Supply of energy and data was to be reliably provided during the articulated arm robot's complex rotary and pivoting movements and vertical strokes. The core of the solution today is a triflex R energy chain that flexibly follows the robot arm on axes 2 to 6. A robust E4/4 energy chain also allows lifting over a 5m travel and allows the system to rotate 380°.

Profile

  • What was needed: triflex R 3D energy chains; E4/4 energy chain
  • Requirements: failure-free supply of a KUKA 125 - 2 with energy and data on axes 1 to 7
  • Industry: aircraft construction
  • Success for the customer: The triflex R flexibly follows the complex movement of the articulated arm robot. A defined bend radius enormously increases the service life of the guided cables and hoses beyond what a cable protection hose allows.
KUKA robots This KUKA articulated arm robot is used in CFRP processing in the aviation industry. A solution was to be found for cable guidance on axes 2 to 7 and for robot lift and rotation.

Problem

As in the automotive industry, everything in aircraft design is based on tight schedules. So it is not surprising that the failure of an expensive machine or a robot not only greatly delays processes, but also means high costs.
For KUKA articulated arm robot cable guidance, CTC-GmbH, a subsidiary of aircraft manufacturer Airbus, was concerned with just this issue. Within the Airbus Group, the company specialises in manufacturing development for carbon fibre reinforced polymer processing (CFRP). For particularly lightweight alternatives to milled metallic components, special processes are being developed to reliably produce even load-bearing parts of the aircraft fuselage with cutting-edge carbon fibre technology.
This is just where the robot in question, a KUKA 125 - 2, comes in. Its tool needed to be supplied with energy and data to perform its tasks.

Solution

Since the robot was also to be equipped with a seventh axis and rotates around its own axis, we delivered several energy supply systems to the Airbus subsidiary.
The key component of the cable guidance solution today is a triflex R energy chain for axes 2 to 6, which move three-dimensionally, that is installed directly on the robot arm. The 3D energy chain flexibly handles the industrial robot's complex, jerky rotational and pivoting movements. A defined bend radius also enormously increases the service life of the guided cables and hoses beyond what a cable protection hose allows.
For the linear motion on axis 7, we recommended installing an E4/4 energy chain on a travel of 5m. The especially versatile cable guidance system is easy to install and has a modular design. In this application, the solution meets the need for an especially robust chain with high rigidity.
The cable guidance for the KUKA robot is rounded off with another E4/4 energy chain for the robot's circular movement on the first axis. This allows rotation of 380°.
KUKA articulated robot The hanging KUKA robot can be rotated 380°. This is accomplished with an E4/4 energy chain on the first axis.
KUKA articulated robot

More on applied products here

Further interesting applications from extremely diverse areas can be found here.


Application Assistance

For further questions or product information, please contact:

Photo
David Sandiland

Robotics and Automotive Industry Sales Manager

Email

Customer Service:

Monday to Friday from 8 am - 8 pm

Online:

24h


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302