Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270
US(EN)

iglide® plastic bushings - surface speed


Table 1.1: Surface speeds (continuous) of iglide® plastic bushings in inch/s

Material Rotating Oscillating Linear
iglide® G300 0.039 0.027 0.157
iglide® J 0.059 0.043 0.314
iglide® M250 0.031 0.023 0.098
iglide® L280 0.039 0.027 0.157
iglide® T500 0.059 0.043 0.196
iglidur® A180 0.031 0.023 0.137
iglide® A200 0.031 0.023 0.078
iglide® A290 0.039 0.027 0.118
iglide® A500 0.023 0.015 0.039
iglide® F 0.031 0.023 0.118
iglide® H 0.039 0.027 0.118
iglide® H4 0.039 0.027 0.039
iglide® H370 0.047 0.031 0.157
iglide® L250 0.039 0.027 0.078
iglide® P 0.039 0.027 0.118
iglide® Q 0.039 0.027 0.196
iglidur® R 0.031 0.023 0.137
iglide® UW 0.019 0.015 0.078
iglide® V400 0.035 0.023 0.078
iglide® T500 0.059 0.043 0.196
iglide® B 0.027 0.019 0.078
iglide® C 0.039 0.027 0.078
iglide® D 0.059 0.043 0.314
iglide® GLW 0.031 0.023 0.098
iglide® H2 0.035 0.023 0.098
iglide® J200 0.039 0.027 0.393
iglide® T220 0.015 0.011 0.039
iglide® UW500 0.031 0.023 0.078


Table 1.2: Surface speeds (short-term) of iglide® plastic bushings in inch/s

Material Rotating Oscillating Linear
iglide® G300 2 1.4 5
iglide® J 3 2.1 10
iglide® M250 2 1.4 5
iglide® L280 2.5 1.8 6
iglide® T500 3.5 2.5 10
iglide® A180 1.2 1 5
iglide® A200 1.5 1.1 3
iglide® A290 2 1.4 4
iglide® A500 1 0,7 2
iglide® F 1.5 1.1 5
iglide® H 1.5 1.1 4
iglide® H4 1.5 1.1 2
iglide® H370 1.5 1.1 5
iglide® L250 1.5 1.1 3
iglide® P 2 1.4 4
iglide® Q 2 1.4 6
iglide® R 1.2 1 5
iglide® UW 1.5 1.1 3
iglide® V400 1.3 0.9 3
iglide® Z 3.5 2.5 6
iglide® B 1 0.7 3
iglide® C 1.5 1.1 3
iglide® D 3 2.1 10
iglide® GLW 1 0.7 3
iglide® H2 1 0.7 3
iglide® J200 1.5 1.1 15
iglide® T220 1 0.7 2
iglide® UW500 1.5 1.1 3

Surface speed

Revolution speed is always significant with plastic bushings. The absolute rotational speed is not decisive, instead it's the relative speed between the shaft and the bushing.

The surface speed is expressed in feet per minute (fpm) and calculated from the rotational speed (rpm) with the following formula:

Rotations: v = rpm x d1 x π/12 = fpm

Oscillating motion: v = 4ab x πd / 360 x 12 = fpm
d1 Shaft diameter (inch)
a Angle of motion either side of the mean position (°)
b Frequency (cycle per min)
d Inner diameter (inch)


Permissible surface speeds

iglide® plastic bushings were primarily developed for low to medium surface speeds in continuous operation.

Table 1.1 shows the permitted surface speeds of iglide® plastic bushings for rotating, pivoting and linear motion.

These surface speeds are limit values under the assumed minimum pressure loads of the bearing. In practice, these limit values are rarely reached due to an inverse relationship between load and speed. Each increase of the pressure load inevitably leads to a reduction of the permissible surface speeds and vice versa.

The speed limit is measured by the bearing temperature. This is also the reason why running speeds differ depending on the type of movement. For linear movements, more heat can be dissipated over the shaft, since the bushing uses a longer surface area.

Surface speed and wear

Considerations about the maximum permissible surface speeds should also include the wear resistance of the plastic bushing. High surface speeds automatically bring correspondingly high wear rates with them.

Surface speed and coefficient of friction

The coefficient of friction for plastic bushings depends on the surface speed. High surface speeds have a higher coefficient of friction than low surface speeds. Figure 1.8 illustrates this relationship in the example of a cold rolled steel shaft with a load of 102 psi with 30 and 59 fpm.
Pillow block bearing test Picture 1.7: Wear and friction tests with the example of an igubal® pillow block bearing
Picture 1.8: Test to determine the maximum surface speeds of an igubal® rod end bearing at high rotational speeds
Figure 1.8: Coefficients of friction of iglide® plastic bushing materials at various surface speeds (Cf53 shaft)

Next chapter



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302