Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270
US(EN)

Inspection device for offshore drilling riser

Drilling risers are used in the offshore oil and gas industry to connect elements between the drilling platform and the seabed. The risers operate under high mechanical loads and in harsh conditions encouraging corrosion and wear. As a result, regular maintenance inspections of the drilling riser must be completed.
The inspection device semi-automatically scans the entire interior of the riser’s main pipe. Its articulated joints are mounted on iglide G300 plastic bushings. These bushings have low friction and are free of stick-slip. The core parts of the sensor mechanism use drylin® N linear slides and igubal® rod ends. Each individual sensor is installed on a drylin® NK-02-27 miniature linear guide. This is then connected to the central adjustment by a self-aligning rod end with either a right- and/or a left-hand thread (EBRM-05 and EBLM-05).

More product information

More application examples from different industries

Useful Links



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302