Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270
US(EN)

Plain Bearings Applied in Bicycle Suspension Shocks

New bike shocks use plain bearings for their low wear rates, light weight, flexibility and to reduce costs

The iglide® RN56 plain bearing was applied to a novel design of bicycle suspension shocks.

To dampen impacts on bicycles, a shock absorber is used between the swing arm rear suspension and frame. Traditionally, this is a cylinder in which a piston moves backwards and forwards in linear motion. The problem is that this type of design can become expensive and add unneeded weight to the bike.

By applying a novel design featuring an individual element made of iglide® RN56 plain bearings as the core piece of the suspension shocks, the technical requirements could be achieved at clearly reduced costs.

The functions of the pistons and the plain bearing at the end of the damper are combined in a single injection-molded component. This is possible thanks to the excellent coefficient of friction and low wear of the iglide® RN56 material. Furthermore, the design allows the piston to be removed from the cylinder, which is of enormous benefit in folding bikes.

Discuss your project with a bearings expert

Whether you're interested in turnkey, fully assembled solutions or looking to build your own customizable project, learn more about how igus® can assist you with a solution based on your specific application and requirements. Contact us via the form below or call us at (800) 521-2747 to discuss your project today!

Contact an igus® expert now



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302