The alternative to the cable drum: igus® e-spool®
Being compact and having a long service life, the system combines the benefits of two different energy supply systems: A standard e-chain from the E2/000 series guides each roll and uses an integrated retaining spring to ensure that the energy supply system has exactly the correct length and tension at all times. The customer can select between three different lengths (0-4 m, 4-7 m and 7-14 m). In the home position, the chain is completely rolled up to save space. Depending on the number of guided cables, the
1400 series e-chain can be ordered with inner widths of 80 and 125 mm.
The
twisterband connects the roll to the shaft block, which is used as the interface to the permanently installed cables. In "classical" cable drums this task is mostly provided by sliding contacts. The e-spool® concept stands out for its significantly higher flexibility. In contrast to sliding contacts, data cables, compressed air lines and fluid lines can also be connected throughout an entire system, and also be exchanged and modified at any time.