igus® tensile tests

tensile test Picture 01
igus® strain relief systems are tested in practice taking into account a variety of parameters.
Whether under the influence of fluids like water or oil, or in the most varied ambient temperatures. The combination of the Chainfix systems with a wide range of jacket materials of cables and hoses plays also of course a role in the in-house tests.

Picture 01: Tensile test igus® CFX clamp with double trough
tensile test Picture 02
Picture 02: Tests for tensile strength with chainflex® cables.
tensile strength test Picture 03
Picture 03: Test on the tensile strength of the igus® chain tie-wrap plate with cable tie.
tensile strength test Picture 04
Picture 04: igus® comparative test of three different strain reliefs - Conclusion: The tensile strength of the igus® Chainfix clamp is more than thrice as high as that of conventional strain reliefs.
tensile strength Tests for tensile strength with chainflex® cables
tensile strength Test for tensile strength of the igus® chain tie-wrap plate with cable tie
tensile strength igus® comparative test of three different strain relief systems - conclusion: The tensile strength of the igus® Chainfix clamp is more than thrice as high as that of conventional strain relief systems.