Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270

Design of a machine tool with highly integrated mechatronic milling module

cable carriers for machine milling This machine can undertake precise milling work with the use of cable carriers

Difficult-to-access workpieces often have to be worked on manually. The German Federal Ministry for Education and Research decided to fund a project to change this so that easy milling tasks can be completed automatically. The resultant prototype machine tool is designed for serial production and enables companies to save both time and money.

The greatest challenge was to combine the advantages of the the new design prototype with the merits of conventional machine tools. Flexibility, movement quality and precision had to be combined in the novel machine tool concept.

igus® came into the picture when the cable running outside the robot had be protected whilst maintaining maximum flexibility. This was achieved using a triflex® R multi-axis cable carrier, with which cables are protected against dirt accumulation and a long service life is guaranteed.

multi axis cable carriers Cable Carriers with long service life

More about applied products


More application examples from different industries