Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270
US(EN)

twisterband

Installation guide for twisterband

TPE outer jacket

Dimensioning: Cable selection

When selecting cables, pay particular attention to good abrasion and gliding properties. An ideal jacket material is TPE.
Recommendation: chainflex® cable CF9
Special shielded cables for the use in twisterband are in preparation. Please contact us if the use of shielded cables is essential

Dimensioning: Filling

twisterband-Version with lock:
TB20-44-18-x-01-0 | TB30-75-22-x-01-0

A = separate cables with crossbars
 
B = Insert cables sorted according to diameter or bending radius. Insert thin, small ones inward – then increasingly bigger ones outward.
 

 

C = Not more than two cables on top of each other. 10% of the larger diameter or a minimum of 1 mm between all cables
 

 

 
D = 10% of the larger diameter or a
minimum of 1 mm between all cables
 

E = 10% of the larger diameter or a
minimum of 1 mm between all cables and separators

twisterband version with easy locking:
TB12-23-09-x-01-0 | TB20-44-12-x-01-0


A = insert cables sorted according to diameter or bending radius. Insert thin, small ones inward – then increasingly bigger ones outward.
 

 

 
B = A minimum of 1 mm or 10% of the larger diameter => Ø B between all cables
 

 

 

 

C = Not more than 2 cables on top of each other. A minimum of 1 mm or
10% of the larger diameter between all cables

Assembly: Mounting brackets

1. Insert twisterband between the steel parts.
2. Secure the twisterband by screwing the mounting bracket in place.

Assembly: guide shaft

Insert a centric shaft as a guide for vertical installation orientations starting at 1500° rotation angles.
Generally, insert a centric shaft as support for horizontal installation orientations.

Assembly: Strain relief

- Strain relief the cables on both ends
- Ensure that the cable tie lock does not point in the direction of the energy chain

Final position:

The twisterband must not be twisted up to the end. To avoid excessive strain on the cables, a min. reserve of 90° must be planned in front of each mounting point.

twisterband®

Installation videos

Part 1
Part 2
Part 3


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302