By supplying harnessed energy supply systems, so-called readychain® systems, igus® offers a solution in which all power and control cables are already inserted during chain assembly (according to the user's specifications).
Another important advantage of the readychain® is that cables from our own tested
chainflex® range are used. Due to the cores wound in bundles, the gusset-filling extruded inner jacket and the outer jacket material — which is optimally matched to the use in the energy chains — the flexibility of these cables can be optimally adapted to the application-dependent bend radius of the energy chains.