Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270
US(EN)

Plastic bearings application in stirring unit of biogas plant

Corrosion-free bearings not affected by liquid media

corrosion of conventional bearings in biogas plant
plastic bearings in stirring unit of biogas plant
corrosion free bearings in biogas plant

A biogas plant stirring unit presents a difficult job for engineers. They need to design a system in such a way that the infiltration of the medium doesn't cause any damage to the bearings. igus® plastic bearings proved not to corrode in the harsh environment of the biogas plant. These corrosion-free bearings are the best solution when building a biogas stirring unit.

More on applied products here

More interesting applications of igus® products across many different industries here