Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270

Search for application examples

Improve technology and reduce costs

For years the igus® motto has been "plastics for longer life®". By this we mean the production of innovative plastic products which reduce maintenance work, achieve technical improvements, at the same time as reducing costs and increasing service life, everything delivered immediately from stock.

Our customers were able to improve the technology and reduce costs in more than 590 applications.
Some examples:

Longest travel in the world - no more downtimes

longest travel in the world  

The e-chain systems® today clearly contribute toward reliability, as system downtime's, for example through cable breaks, are reduced to zero.

Cables defy heat, sun, rain and snow

Chainflex  

Previously used cables from a competitor had failed; since then the temperature-resistant Chainflex® cables are used; the larger-than-life size LED screen in Dallas functions in any weather.

Rough environment, high speed

chainflex  

Even in particularly aggressive ambient conditions like in this high speed machining center, energy supply systems prove their reliability.

Costs saved, machine
availability increased

iglide  

As iglide® plain bearings have a long service life, and in addition need not be lubricated and costs only a fraction compared to conventional bearings, 90% of the costs could be saved.

More than Euro 10,000 saved each year

igubal  

The previously used bearings were blocked and the shafts used to break. The self-lubricating igubal® flange bearings used instead have been operating since May 2007 without failure. This saved Euro 2,440 in repair costs and Euro 8,400 in machine stoppages each year.

Trouble-free operation instead of shaft destruction

drylin applications  

Due to the dirt accumulation in the ball bearings, the balls were blocked and the shafts were destroyed. The concrete cutting machine has now run for over three years entirely free of troubles despite the extremely heavy-duty operation.

Search

Are you looking for practically tested application examples in a certain industry?
Here you can browse through already implemented applications and filter them according to your specifications.

Industry sector:
Case of application:


Suspended articulated arm robot

Triflex® R as a complete solution for several tasks at once on a suspended robot

Suspended articulated arm robot    

Screen facade for primary school

For wind and rain

Screen facade for primary school    

Bank of lamps

This pivoted bank of lamps is equipped with 32 lamps, 4,000 Watts.

Bank of lamps    

Bucket wheel stacker

This contribution also concerns a circular application that has been designed with an igus® energy chain with rearward bending radius.

Bucket wheel stacker    

Test rig for solar systems

This test rig was able to be built thanks to the use of igus® e-chains®.

Test rig for solar systems    
Applications overview

I have the following project - following question - following request

No application example has been found here for your special case of application. Would you like to have further assistance?
Please let us know how we can help you!



Your data

Please always complete the fields marked *.

Company:*
First name:*
Last name:*
Phone:
Email:*
If you would like to request catalogs or samples then please complete your address here.
Salutation:
Street:
City:
State:
Zip code:
Country:
Yes, I would like to be included on the igus® Newsletter list.
I agree to the data protection regulations and the processing of my data. You can revoke this authorisation at any time.
Send