Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270
US(EN)

Linear bearing and housing unit use in leak test stand

Linear bearings and housing unit are maintenance free and cost-efficient solution

To make the leak stand test (quality control test for a heat exchanger) work, a facility required a guide with the following properties: sensitive to dirt, maintenance-free, water-resistant, vibration-resistant and cost-efficient. drylin® linear bearings and a housing unit were installed. Two drylin® quad blocks (RQA 01-30) and four shaft end supports (TA-30) were used (as pictured below). The facility has been in operation for many months and the igus® elements have proven themselves as the perfect solution.
Linear Bearing & Housing Unit in leak test stand
close-up of bearing shaft-end supports
"To realize this function, we required a guide with the following properties: sensitive to dirt, maintenance-free, water-resistant, vibration-resistant and cost-efficient! Two drylin® quad blocks (RQA 01-30) and four shaft end supports (TA-30) were used. The facility is already in operation for many months; the igus® elements have proved themselves. ”

Michael Zimmermann, Möve-Metall GmbH, Mühlhausen

More on applied products here

More interesting applications of igus® products across many different industries here



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302