Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270
US(EN)

iglide® Bearings in Fishing Spearguns

Spear fishing is a popular sport at coastal regions all over the world. The speargun is essentially the same everywhere in that it comprises a long tubular or solid wood frame, a trigger mechanism and a long, slender spear. Rubber straps are stretched by pulling them with both hands and a steel wishbone is hooked over a notch in the spear. Varying strengths of rubber are available providing varying force and therefore distance traveled of the spear. Multiple straps may be used where the required force is too great for the user to load effectively. Only very practiced spear fisherman are able to load their guns quickly and therefore take advantage of stronger rubbers. The traditional method of loading requires that the butt of the gun is pushed into the stomach or hip while the biceps are required to produce all of the pulling power. This is difficult enough to achieve on land, let alone in the water. It is also essential that the procedure is performed quietly so as not to scare the fish away.

It was therefore decided to develop an alternative method of loading the gun utilizing the much stronger, leg muscles. After several early concepts, the present idea was born which utilizes a travelling rubber strap mount which slides along the barrel and can be latched into place at its end. A second sliding member with rotating posts is used to push the former mount along the barrel. The rotating posts are positioned 180 degrees apart and pressed on with the heels of the feet. Once the rubber strap mount is latched in, the 'foot slider' can be pulled back towards the trigger end and the posts rotated downwards to be held with the non trigger hand for increased stability. From the outset, the choice of bearing type for the sliding members was of paramount importance. Factors such as minimal friction, corrosion resistance and quietness were all considered.

In the end and after testing, the choice was made in favor of iglide® H370 plastic bearings. These have excellent chemical properties and are actually recommended for underwater use. The barrel is a PTFE coated aluminium tube, which complements the igus® bearing perfectly. The end result is a highly effective speargun which can be effectively loaded. The stronger rubbers can be utilized by less experienced fisherman, giving them the sport enjoyment of their peers.

"Predicted lifetime of the gun looks good with very low wear rates. Importantly, the gun is extremely quiet in use. This could not have been possible without the use of advanced plastic bearings such as those produced by igus®. Roll on next summer!" - Jon Prince, Design Engineer at The Design Village

Browse Applicable Products

iglide® H370

iglide H370 sleeve bearing
  • Extremely long service life under water and high media-resistance
  • Wear-resistant – especially under water
  • High temperature resistance –104 °F to +392 °F
  • High chemical resistance
Shop now

Discuss your project with a bearings expert

Whether you're interested in turnkey, fully assembled solutions or looking to build your own customizable project, learn more about how igus® can assist you with a solution based on your specific application and requirements. Contact us via the form below or call us at (800) 521-2747 to discuss your project today!

Contact an igus® expert now



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302