Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270
US(EN)

Bearings Improve Artificial Knee Joint

Download the PDF version of this application story

Plastic bearings used for improved performance

A leading worldwide supplier of orthopedic technology for the past 90 years offers sophisticated, top-quality products and services to people with restricted mobility. By using plastic bushings, instead of needle or bronze bearings, the company’s artificial knee-joint design was significantly improved. Metal bearings proved to be susceptible to dust and dirt and developed disturbing noise with increased play and significant wear. The challenge was to find a plain bearing which could operate without the need for any maintenance or play. They should also run noiselessly, cushion impacts and have a good cost/performance ratio. iglide® L280 and iglide® Q plastic bushings from igus® are situated in all the bearing points of the artificial knee joint.

iglide® L280 plastic bushings have low coefficients of friction and extremely high wear resistance. They are suitable for soft shafts and withstand chemicals. iglide® L280 also has a very high compressive strength, despite high elasticity. Under the maximum permissible load of 8,702 psi, the deformation at room temperature is less than 3 percent. The coefficients of friction also do not increase with higher surface speeds. Compared to other materials, it can achieve slightly higher surface speeds - for instance up to 4.9 ft/s during rotating movements and up to 16.4 ft/s during linear movements. Due to the exceptional wear resistance, bearing wear remains low even long term even at high speeds on hardened shafts. For minimum coefficients of friction with iglide® L280, the surface should not be too smooth.
plastic bushing on artificial knee joint Artificial knee joint

Fit for high loads

If very high loads are involved, iglide® Q bearings are generally recommended, as they were developed especially for such applications. With a radial load of 3,626 psi, they even surpass bearings made from highly wear-resistant iglide® L280. Under the maximum permitted load of 14,504 psi, the elastic deformation at room temperature is less than 3 percent.

iglide® Q plastic bushings offer the greatest advantages in terms of high loads and low speeds. Due to their excellent coefficient of friction, high surface speeds are also possible. iglide® Q bearings retain their excellent wear resistance at high temperatures as well. The permissible long-term application temperature is 302°F.

The artificial limb is now lighter and smooth-running thanks to the implementation of plastic bushings. The patient need only rarely visit an orthopedic mechanic.
plastic bearings These bearings are known as the "endurance runners" among the igus® products.

Browse Applicable Products

iglide® L280 bearing

artificial knee joint uses iglide L280
  • Specially made for fast rotating applications
  • Long service life & low coefficient of friction
  • Extremely high wear resistance
Shop now

iglide® Q bearing

artificial knee joint uses iglide Q bearing
  • Excellent wear resistance, especially for extreme loads
  • Recommended for extreme pv values
  • Good coefficients of friction
Shop now

Discuss your project with a bearings expert

Whether you're interested in turnkey, fully assembled solutions or looking to build your own customizable project, learn more about how igus® can assist you with a solution based on your specific application and requirements. Contact us via the form below or call us at (800) 521-2747 to discuss your project today!

Contact an igus® expert now



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302