High loads
In fact, all the mountings on this innovative vehicle use iglide® plastic bushings, with the exception of the wheel bearings which use ball bearings.
iglide® Q plastic bushings are particularly well-suited to heavy-duty applications: they cope well with high loads and different pivoting angles.
Even in tough environmental conditions - like those encountered by an electric scooter out on the road - the igus® bushings are extremely wear resistant. This includes sub-zero temperatures, as well as heat and humidity. Even hard impacts as a result of potholes in the road, or the continuous vibrations do not affect the functionality of bushings.