Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270
US(EN)

Jetpack

Very hot

The Jetpack with igus® products presented here gets closer to the dream of flying. The “pilot” has a rocket drive buckled to his back that will give him the required thrust. Since temperatures of several hundred degrees Fahrenheit occur here, the pilot must wear fire and heat-resistant clothing. The bearings used also have to withstand the high temperatures and pressures. Various iglide® plain bearings are used in the overall construction, and xiros® plastic ball bearings are used on the control handles. In addition, the most important connection for the whole control system is an igubal® rod end bearing which bears the pilot’s whole weight.

Applied propulsion, Mario Böhme, Gross-Zimmern, Germany

Jetpack using igus iglide bearings, xiros ball bearings and igubal rod end bearings.
Jetpack using igus iglide bearings, xiros ball bearings and igubal rod end bearings.

More on applied products can be found here.

More applications from different sectors can be found here.



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302