Note: RSE wheel bracket arrangement can be modified to opposite side if needed. Remember to keep mounting feet on the same side as the glide-through bracket
Mounting adapter
Mounting adapter installation example
Retraction system installation
Align the mounting feet with the mounting adapter holes.
Bolt mounting feet to mounting adapter.
Axis 6 installation
Tennis racket (axis 6 clamp) installation
Tennis rackets available for most robot models.
Bolts need to be tightened uniformly.
Can be mounted in any direction.
Standard and Heavy-duty brackets
Adjustable in four directions
Designed with integrated profile rail for CFX clamp
Axis 6 bracket installation
Install the bracket as close to the end of the handle as possible and tighten the bolts equally.
triflex® R installation
Cable installation
Easy cable installation possible with triflex® TRE and TRCF only.
If using TRC, cables will need to be fished through individually
Install locking clips
triflex® TRE only - install locking clips at each fixed bracket position
Ball end of triflex® R at the EOAT (End of arm tooling)
Install triflex® R
Install triflex® R in axis 6 mounting bracket first.
Make sure triflex® R is not twisted.
Installing CFX clamps
Install CFX clamps to secure cables.
Installing protectors
To pretension the system, pull the triflex® forward two links and install a protector at the exit of the moving end.
For quick release protectors, use a flat head screwdriver to pry the two halves apart
Installing protectors
Install protectors where triflex® R makes contact with the robot.
triflex® RSE WHEEL troubleshooting guide
Problem
Solution
triflex® R breaks when RSE System is fully extended
Install more triflex® R outside the RSE System. The motion of the robot is greater than the available travel of the RSE System
RSE System does not function
Ensure the bands have tension
Confirm that the system is free of debris
Reduce the length of the triflex® R outside the RSE System
Carriage slams when the robot returns to the hom position
Pull the system forward four links and install a protector at the exit of the pass-through bracket thereby creating a stop
Discuss your project with a triflex® R expert
We can assist you with a turnkey, fully assembled solutions or answer any questions you may have with a custom project.
David Sandiland Robotics Sales Manager - North America (705) 313-2574