Solution
Mr. Janosz confirms that by guiding the hoses and cables with the help of TRE.40.058.0.B, the problems mentioned above have been eliminated. According to him, the robot now moves "much more freely, almost gracefully". According to IEC sp.zo.o., "Every Cobot should be equipped with this solution as standard". Cobots react very sensitively to increased tension or pressure, which is controlled by the correct cable guidance using TRE.40.058.0.B. From now on the cable ties are used for the correct strain relief and not for fixing the cables and hoses.
Configure now