Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270
US(EN)

Examination of wear against a customer's shaft made of 1.4034

Since the application run-time of iglide® Z required by a customer on a shaft made of 1.4034 steel could not be reached, we re-enacted this case in our test lab in order to find a more suitable iglide® material.
 
These were shafts, such as those used by the customer, made from the material 1.4034. Then different plain bearings were tested against these shafts, in order to obtain a better combination with the shaft material.
 
The wear comparison was carried out under the following test parameters:Force: 3,626 psi
Speed: 0.039 f/s
Run-time: 100 h
Shaft: 1.4034
Plain bearing materials: iglide® Z, iglide® J350, iglide® P210, igus® development material, DU with PTFE layer
Examination of wear against customer's shaft Rotating wear

Result:

The lowest wear rate could be achieved in combination with an iglide® material still under development. The best among those available is the iglide® J350 material. With a wear rate of 26.8 µm, the iglide® J350 bearing has less wear than iglide® Z by more than 33%.

Do you wish to test a custom application?

We will gladly test your specific application as well. Simply use the contact form on the back!

More information:

iglide® J350 - Material data

iglide® J350 - High wear resistance in rotation

Now you may order the winner of the test:

dry -tech® test laboratory

In the dry-tech® test laboratory about 135 trillion test movements are conducted every year.


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302