Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270
US(EN)

Artificial Limb Absorbs Shocks and Impacts

Amputees will attest to the importance of comfort above all other factors for a successful prosthesis. Daily activities involve frequent impacts and rotational movement.

Whereas a rigid prosthesis transfers these forces directly to the body interface - causing discomfort - one company’s unique lower limb prosthesis absorbs and reduces them in a resilient rod-and-spring action.

The energy-and-torque managing device originally used a PTFE mesh bearing, which was molded into the surface of a carbon-fiber tube. However, the bearing surface suffered significant wear when subjected to high loads, which resulted in play unacceptable to an amputee.

An iglide® Z plastic bushings from igus proved to be the only bearing able to withstand the significant edge loads and shear forces produced by patients weighing up to 275 lbs.

The finished prosthesis can be used when walking, running or even when taking part in extreme sports. Wearers attest to a smoother, more reliable motion and feel.
Energy-and-torque managing device
Prosthetic limb can be used in many daily activities


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302