Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270
US(EN)

iglide® L280 - Material data

Materials table

General features Unit iglide® L280 Test method
Density g/cm³ 1.24
Color Yellow
Max. humidity absorption at 73° F/50% R. H. Wt.-% 1.3 DIN 53495
Max. water absorption Wt.-% 6.5
Coefficient of surface friction, dynamic, against steel µ 0.08 - 0.23
p x v value, max. (dry) psi x fpm 6,600

Mechanical properties
Modulus of elasticity psi 507,600 DIN 53457
Tensile strength at 68° F psi 18,130 DIN 53452
Compressive strength psi 8,847
Permissible static surface pressure (68° F) psi 8,702
Shore D hardness 77 DIN 53505

Physical and thermal properties
Max. long-term application temperature °F 194
Max. short-term application temperature °F 356
Min. application temperature °F -40
Thermal conductivity [W/m x K] 0.24 ASTM C 177
Coefficient of thermal expansion [K-1 x 10-5 ] 9 DIN 53752

Electrical properties
Specific volume resistance Ωcm > 1013 DIN IEC 93
Surface resistance Ω > 1012 DIN 53482

Permitted p x v values

For iglide® L280 plastic bushings with 0.03937 (1 mm) wall thickness in dry operation against a steel shaft, at 68° F, installed in a steel housing.

High wear resistance, particularly in environments with abrasive media or in connection with coarse shafts, distinguishes the iglide® L280 material. Among all iglide® materials, this is the most insensitive to such external influences.

Deformation under load and temperatures Figure 5.2: Deformation under load and temperatures

Compressive Strength

iglide® L280 shows a very high compressive strength despite high elasticity. Figure 5.2 shows the elastic deformation of iglide® L280 with radial loads. Under the maximum recommended surface pressure of 8700 psi, the deformation at room temperature amounts to less than 3%.

A plastic deformation at room temperature is practically negligent within the maximum recommended surface pressure of 8700 psi.

Maximum surface speed

fpm Rotating Oscillating Linear
Constant 196 137 787
Short-term 492 354 1181

Permitted surface speeds

Even at higher surface speeds, the coefficients of friction of iglide® L280 plastic bushings do not increase. Therefore compared to other materials it can attain slightly higher surface speeds, for instance up to 295 fpm rotating and up to 984 fpm linear.

Due to the extraordinary wear resistance, the bushing wear remains low also in long-term application with high speeds.

Extremely high speeds can be attained with iglide® L280 plastic bushings on hardened, not too smooth shafts.

Temperature limits

iglide® L280 Application temperature
Lower - 40 °F
Upper, long-term + 194 °F
Mechanically secured + 266 °F
Upper, short-term + 356 °F
Additional axial securing + 140 °F

surface pressure for plastic bushings Figure 5.3: Maximum recommended surface pressure dependent on the temperature

Temperatures

iglide® L280 plastic bushings are extremely insensitive to alternating external influences. This applies also to temperatures. iglide® L280 plastic bushings retain their extraordinary abrasion resistance even up to the maximum permitted application temperatures and do not tend to become brittle at low temperatures.

In contrast the mechanical properties limit the usability of iglide® L280 at high temperatures. A relaxation of the bushings can occur at temperatures of 176° F. In the process the bushing's press-fit force can reduce so strongly that with re-cooling and the entailing shrinking, the bushing can creep out.

In order to prevent this, in applications from 140° F the iglide® L280 plastic bushings should be certainly mechanically secured in addition.

Coefficients of friction for iglide® L280 against steel
(Shaft finish = 40 rms, 50 HRC)

iglide® L280 Dry Grease Oil Water
Coefficients of friction µ 0.08 - 0.23 0.09 0.04 0.04

coefficients of friction Figure 5.4: Coefficients of friction dependent on the surface speed, p = 108 psi, shaft made of Cold Rolled Steel

Friction and wear

The coefficients of surface friction of the iglide® L280 decreases with increasing load. In dry operation paired with steel (Cold Rolled Steel), they reduce by about 25% just in the load range of p = 72.5 to 507.5 psi.

In contrast to other iglide® materials, the coefficient of friction of the iglide® L280 remains constantly low even at higher peripheral speeds.

Friction and wear also depend to a high degree on the reverse partner. Very smooth shafts increase the coefficient of both friction and wear. Smooth shafts entail the danger of stick-slip. The squeaking noise as an effect of stick-slip is often the result of extremely smooth shafts. Please note that a smoothing of the shaft surface can also occur due to the operation.

For minimum coefficients of friction with iglide® L280 plastic bushings, the shaft surface should not be too smooth. Shaft surface finish of 16 to 20 rms are the ideal (see Fig. 5.6) For the iglide® L280, the wear resistance is still excellent with this surface finish as the friction adopt the minimum value.
load of bushing Figure 2.5: Coefficients of friction dependent on the load, v = 1.97 fpm
shaft surface bearing Figure 5.6: Coefficients of friction dependent on the shaft surface (shaft Cold Rolled Steel)

bushing loads Fig. 2.7: Wear, rotating application with different shaft materials, load p = 108 psi
rotating bushings Figure 5.8: Wear with various shaft materials in the rotating operation dependent on the load
pivoting bushing application Figure 5.9: Wear with pivoting and rotating applications with shaft material Cold Rolled Steel dependent on the load

Shaft materials

The diagrams display a summary of the results of tests with different shaft materials conducted with bushings made of iglide® L280.

In rotating applications the wear shows variations indeed according to the shaft at low loads, but the iglide® L280 displays excellent to acceptable coefficients of wear with all tested shafts. iglide® L280 like hard shafts. The iglide® L280 is the most suitable iglide® material at low radial loads and with hard-chromed shafts and hard shafts made of corrosion-resistant steel (X90). The soft shaft materials ST37 and machining steel are not as suitable for the iglide® L280 bushings.

At high loads, hardened shafts should be chosen. Diagram 5.8 clearly shows the differences with rising loads. A similar picture emerges in pivoting applications. With initial low loads, the wear for the pivoting motion lies actually lower than that for a rotation at the same load. This picture changes with higher loads.

Please contact us in case the shaft material scheduled by you is not included in this list of tested glide partners.

Important tolerances for iglide® L280 plastic bushings according to ISO 3547-1 after the press-fit.

Diameter
d1 [inches]
Shaft h9
[inches]
iglide® W300
E10 [inches]
Up to 0.0197 0 - 0.000984 +0.0005512 + 0.0021260
> 0.1181 to 0.2362 0 - 0.001181 +0.0007874 + 0.0026772
> 0.2362 to 0.3937 0 - 0.001417 +0.0009842 + 0.0032677
> 0.3937 to 0.7087 0 - 0.001693 +0.0012598 + 0.0040157
> 0.7087 to 1.1811 0 - 0.002047 +0.0015748 + 0.0048819
> 1.1811 to 1.9685 0 - 0.002441 +0.0019685 + 0.0059055
> 1.9685 to 3.1496 0 - 0.002913 +0.0023622 + 0.0070866
> 3.1496 to 4.7244 0 - 0.003425 +0.0028346 + 0.0083464
> 4.7244 0 - 0.003937 +0.0033464 + 0.0096456

Installation tolerances

iglide® L280 plastic bushings are standard bushings for shafts with h-tolerance (recommended minimum h9). After the installation in a housing bore with the H7 tolerance, the inner diameter of the bushing automatically adjusts to the E10 tolerance.

Medium Resistance
Alcohol + to 0
Hydrocarbons, chlorinated +
FGreases, oils, without additives +
Fuels +
Diluted acids 0 to -
Strong acids -
Diluted bases +
Strong bases 0
+ resistant      0 conditionally resistant      - non-resistant

bushings in humidity Figure 5.10: Influence of moisture absorption of iglide® L280 bushings


Electrical properties

Specific volume resistance > 1013 Ωcm
Surface resistance > 1012 Ω

Chemical resistance

iglide® L280 plastic bushings have a good resistance against chemicals. They are resistant to most lubricants. iglide® L280 is not affected by most weak organic and inorganic acids.

The humidity absorption of iglide® L280 plastic bushings amounts to about 1.3 Wt.-% in standard climatic conditions. The saturation limit in water is 6.5%. This should be considered according to environmental influences.

Radioactive rays

iglide® L280 plastic bushings are radiation resistant up to a radioactive intensity of 3 x 10² Gy.

UV-resistant

iglide® L280 plastic bushings are permanently resistant against UV rays. A minor variation in the color (dark) through UV radiation and other atmospheric exposures influences the mechanical, electrical or thermal properties only insignificantly.

Vacuum

The potentially absorbed humidity of the iglide® L280 plastic bushing degasses in vacuum. The application in vacuum is therefore possible only restrictedly.

Electrical properties

Plastic bushings made of iglide® L280 are electrically insulating.


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302