More and more series converted
The first tests were carried out to the complete satisfaction of both the L&K engineers and the users. The ultra-light design, which is supplemented by
iglide® plain bearings, is protected by a utility patent. It is used in a wide variety of applications, such as high dump buckets, which are used as salt loading buckets in the salt depots of municipal utilities, and in various designs of grab buckets and trench buckets. For a high dump bucket with a capacity of 8.5 m
3, L&K has already implemented a real "XXL application" for the maintenance-free iglide® plain bearings several times.