Cables and hoses
Two important factors in vertical cable management are how the conduits lay in the energy chain cable carrier and and how they are secured at the end points: All
cables and hoses must be hung so that they bear their own weight. The energy chain fulfills the function of orderly conduit bundling only and should not absorb any further tensile forces. igus® interior separation elements should be used for distinct division of all cables and hoses. The cables and hoses must be secured carefully to both end points of the energy chain. The
strain relief must be designed so that the opposite run cannot catch.