Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270
US(EN)

FDA-compliant, stainless steel ball bearings in guide rollers for conveyor belts

Elimination of lubrication, long service life, hygienic design, suitability for intensive cleaning processes and anti-static component properties are indispensable in packaging technology. GEA Food Solutions Germany GmbH invested in our construction kit and equipped its machines with linear bearings, plain bearings ball bearings and drive elements.

Application Overview:

 
  • What was needed?  Electrostatically dissipative ball bearings
  • Requirements: Electrostatic conductivity, freedom from lubrication and maintenance, FDA-compliant
  • Material: xirodur F180
  • Industry: Packaging technology
  • Success for the customer:  xiros plastic ball bearings have no complicated sealing concepts, therefore the bearings run continuously and without problems. xirodur F180 also provides the required electrostatically conductivity.
xiros® plastic ball bearings in packaging technology

Problem:

The problem was the conventional metal ball bearings used in the film guide rollers. They usually caused sparking, which should be avoided in packaging technology. Complicated sealing concepts that use lubricants also make metal ball bearings a food contamination hazard. The search focused on an electrostatically dissipative, lubrication-free alternative that operated smoothly.

Solution:

The solution for the film guide rollers was xiros ball bearings made of the xirodur F180 high-performance plastic. These bearings are not only 100% self-lubricating, but also ensure that sparks are obsolete due to the polymer used. The combination of polymer housing and stainless steel balls ensures  maintenance-free operation, and  FDA approval shows that it is suitable for food packaging. 

Browse the Shop:

Radial deep groove ball bearing

radial deep
  • xirodur F180, stainless steel balls, cage made of PE
  • Food-safe, FDA and ESD-compliant
  • Smooth-running, dirt-resistant
  • Very little humidity absorpton
Browse the Shop


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302