Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270
US(EN)

Plastic ball bearings used in water generators at a hydropower plant

Application Overview:  The customer had a plant for converting wave energy into electric energy by means of floats arranged in a line. Within these floats was a mechanism that converted the up-and-down movement into electrical energy . A cable then transferred the energy to land.

What was needed? 
Bearing support that increases service life and eliminates maintenance.
  • Requirements: Dimensional stability, no lubrication, corrosion resistance
  • Material: xirodur B180
  • Industry: Hydropower, Fluid Technology
Success for the customer:
With xiros plastic ball bearings, the encapsulation that would normally have been necessary for metal ball bearings was dispensed with. 
xiros® plastic ball bearings in water generators

Problem

Because the system is continuously used in seawater, the customer was looking for a bearing that would increase system service life and eliminate maintenance. Due to waves, high lateral forces, called drift forces act on the float. The floats must be strong, low-friction and use as little lubricant as possible.

Solution

The pivot points outside the float, provide great stability against the drift forces caused by the waves. But this means that the joints are exposed. By switching to xiros polymer ball bearings, the customer was able to eliminate the enclosures necessary in conventional rolling bearings. Seawater flows through the polymer ball bearings and there is no risk of water polluting substances leaking through a bearing enclosure.

Browse the Shop

Radial deep groove ball bearing

xiros BB
  • Material:  xirodur B180
  • Stainless steel ball
  • Smooth running, dirt-resistant
  • Very little humidity absorption
Browse the Shop


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302