Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270
US(EN)

Stainless steel guide rollers with xirodur® A500 ball bearings

Temperature-resistant xiros® guide roller made of stainless steel

For chemicals and heat

These stainless steel guide rollers can be used without any reservation in environments where temperatures are consistently as high as 302°F. The secret is the high-temperature ball bearings made of xirodur A500. This special material can be employed not only where temperatures are high, but wherever chemicals are used. Many of our customers in the food and chemicals industries are already using this technology. One example from the food industry is in artificial sausage skin manufacture, where drying areas experience high temperatures, and ball bearings made of other materials are not well-suited.
Tech up

Tech up

  • Operating temperature up to 302°F
  • Individual components with FDA-compliant materials
  • Resistant to a wide range of chemicals
Cost down

Cost down

  • Costs up to 40% less than lubricated metallic ball bearings thanks to the longer service life
Recycling

Sustainability


Self-lubricating endurance runner

Plastics are not necessarily incompatible with hot temperatures, as the Koppe example, below, shows. The pellet stove's operation is simple and ingenious. A mechanical drive unit moves the pellets without electrical energy through a cylinder resting on a roller into the combustion chamber for a burning time of around 24 hours. For the production process, Koppe was therefore looking for bearings for the drive mechanism that would work in adverse conditions without malfunctioning. The solution the company found was xiros polymer ball bearings made of temperature-resistant xirodur A500. This special material even allows brief high-temperature applications of up to 599°F, and because it needs no external lubrication, it runs smoothly over long periods. Metal ball bearings were out of the question. They seized immediately and generated an immense noise load.
Mechanical drive unit in the Koppe pellet stove
"We thought for a long time about the drive system and how to improve its running performance. We were looking for bearings for the drive mechanism which could work continuously in an adverse environment. The lubrication-free ball bearings play an important role here."
 
Franz Koppe, CEO of Erwin KOPPE – Keramische Heizgeräte GmbH

Innovation presentation


Discuss your project with a xiros® expert

Whether you're interested in turnkey, fully assembled solutions or looking to build your own customizable project, learn more about how igus® can assist you with a solution based on your specific application and requirements. Contact us via the form below or call us at (800) 521-2747 to discuss your project today!

Contact an igus® expert now



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302