Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270
US(EN)

triflex® RSE Wheel

installation guide

Configuring the retraction system

RSE wheel bracket arrangement click to enlarge

RSE wheel bracket arrangement

Note: RSE wheel bracket arrangement can be modified to opposite side if needed. Remember to keep mounting feet on the same side as the glide-through bracket
Mounting adapter installation example click to enlarge

Mounting adapter

Mounting adapter installation example
Retraction system installation click to enlarge

Retraction system installation

  • Align the mounting feet with the mounting adapter holes.
  • Bolt mounting feet to mounting adapter.

Axis 6 installation

Tennis racket (axis 6 clamp) installation click to enlarge

Tennis racket (axis 6 clamp) installation

  • Tennis rackets available for most robot models.
  • Bolts need to be tightened uniformly.
  • Can be mounted in any direction.
Standard and Heavy-duty brackets click to enlarge

Standard and Heavy-duty brackets

  • Adjustable in four directions
  • Designed with integrated profile rail for CFX clamp
Axis 6 bracket installation click to enlarge

Axis 6 bracket installation

Install the bracket as close to the end of the handle as possible and tighten the bolts equally.

triflex® R installation

Cable installation click to enlarge

Cable installation

  • Easy cable installation possible with triflex® TRE and TRCF only.
  • If using TRC, cables will need to be fished through individually
Install locking clips click to enlarge

Install locking clips

  • triflex® TRE only - install locking clips at each fixed bracket position
  • Ball end of triflex® R at the EOAT (End of arm tooling)
Install triflex® R click to enlarge

Install triflex® R

  • Install triflex® R in axis 6 mounting bracket first.
  • Make sure triflex® R is not twisted.
Installing CFX clamps click to enlarge

Installing CFX clamps

  • Install CFX clamps to secure cables.
Installing protectors click to enlarge

Installing protectors

  • To pretension the system, pull the triflex® forward two links and install a protector at the exit of the moving end.
  • For quick release protectors, use a flat head screwdriver to pry the two halves apart
Installing protectors click to enlarge

Installing protectors

  • Install protectors where triflex® R makes contact with the robot.

triflex® RSE WHEEL troubleshooting guide

ProblemSolution
triflex® R breaks when RSE System is fully extended
  • Install more triflex® R outside the RSE System. The motion of the robot is greater than the available travel of the RSE System
RSE System does not function
  • Ensure the bands have tension
  • Confirm that the system is free of debris
  • Reduce the length of the triflex® R outside the RSE System
Carriage slams when the robot returns to the hom position
  • Pull the system forward four links and install a protector at the exit of the pass-through bracket thereby creating a stop

Discuss your project with a triflex® R expert

We can assist you with a turnkey, fully assembled solutions or answer any questions you may have with a custom project. 

David Sandiland
Robotics Sales Manager - North America
(705) 313-2574
Contact an igus® expert now

Overview of Assembly Instructions for igus® e-chains®



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302