Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270
US(EN)

New chainflex® products 2024

Tech up, cost down. It's our job.

Our flexible chainflex cables generally come with a guarantee of up to 4 years, as are our many new products this year. We would like to present extensive additions to the drive technology range. You will also find innovations from the product range for top drive applications and for applications in very dry environments.


CF guarantee

4-year guarantee - there's never been anything like it ...

... 12 additional months for more safety

The unique chainflex guarantee has been extended by another 12 months and is now valid for 4 years! Numerous tests in the 3,800m² test laboratory make such a guarantee possible!

UL-listed cables

chainflex® - UL-listed flexible motor and control supply cables ...

... for the e-chain® and the cable tray

UL-listed flexible motor and control supply cables for use in the e-chain and the cable tray. These listed motor and control cables are ideal for continuous movement and for a seamless transition from the chain to the platform.

CFCLEAN-40million

Securely suspended in the top drive ...

... operational safety in the onshore and offshore sector

The CFSPECIAL.572 has been added to the product range for suspended top drive applications, including DNV approval for use in the maritime sector.

CF-PVC cables

For dry environments ...

... flexible cables with PVC outer jacket

Our new PVC cables are the right choice for oil-free applications. Typical sectors include woodworking, packaging and material handling. 

CFCLEAN-40million

chainflex® CFCLEAN with a guarantee of 40 million double strokes ...

... even more safety for cleanrooms

Increase in the guaranteed service life of CFCLEAN cable elements to 40 million double strokes and simultaneous increase in current-carrying capacity. 

PTFE-free

chainflex® is PTFE/PFAS-free ...

... operational safety guaranteed and confirmed worldwide

chainflex dispenses with PTFE! The new logo confirms the elimination of PTFE in igus chainflex cables. If a general ban is announced, no chainflex cables will have to be disposed of or replaced and can continue to be used worldwide without any concerns.

CFCASE-refill

chainflex® CASE Refill ...

... replacing cables made easy

Thanks to a refill element, the chainflex CASE shipping and storage solution is even more practical and sustainable. Available for both CASE sizes, it allows users to unwind the cables directly from the box.

Cross-section extension

Cross-section extensions for six chainflex® cable series ...

... tested in the chainflex® laboratory and with a guarantee

Six cable series with new cross sections were added to the chainflex product range. Our cables come with the unique chainflex guarantee and have been tested in our own test laboratory.

CF38.O.PE

New high-end motor cable CF38 without protective conductor ...

... resistant thanks to the TPE outer jacket

With the high-end motor cable series CF38, installation space can be saved and at the same time low temperatures down to -35°C can be withstood. With the new cross sections, we are expanding the CF38 family and at the same time replacing the discontinued models of the CF35.UL.

CF340.100.01

The solution for tight installation spaces and long travels ...

... thanks to TPE high-end single-core cable

The new CF340.100.01 is an addition to the CF340 single-core family and, thanks to the robust TPE outer jacket, is ideal for small installation spaces in the energy chain and long travels. 

CF211.030

Encoder cable now also for SIEMENS SINAMICS V90 ...

... specifically developed for dry environments

The CF211 encoder cable series has been expanded for the SINAMICS V90 drive system. Robustness for dry environments is guaranteed thanks to the PVC jacket. The new chainflex CF211.030 is available from stock sold by the metre or harnessed ready for connection. 

CFROBOT8.PLUS

A robot cable with a torsion angle of up to
+/- 360°/m ...

... for CAN bus and Ethernet up to CAT7

The service life of the CFROBOT8.PLUS has been increased by the larger torsion angle of up to +/- 360°/m and solves problems in tight installation spaces.

CF98.PLUS and CF99.PLUS

An unprecedented service life guarantee ...

... CF98.PLUS and CF99.PLUS guaranteed with 100,000,000 double strokes

The new CF98.PLUS and CF99.PLUS control cables achieve the longest durability with 100,000,000 double strokes or a bending factor of 3xd. 

CF280.UL.H401.07.04.D

New hybrid cable CF280.UL.H401 ...

... extended for the ctrlX DRIVE system from Bosch Rexroth

Suitable for drives of the MS2N series from Bosch Rexroth, you reduce costs by 50% and receive the usual service life guarantee. 

CF220.UL.H304

New hybrid cable with PVC outer jacket ...

... for SINAMICS 210 drives ...

With the new PVC hybrid cable, we are adding to the CF220.UL.H cable series and thus offer even more variety. Thanks to the high-quality PVC outer jacket, you can save 15.3% of costs.

CFSPECIAL.5XX with DNV

Special top drive cable solutions ...

... now with DNV approval

With the new DNV approval, the CFSPECIAL.5XX series is the perfect solution for offshore drill rig applications.




The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302