Components across nearly all
marine applications will come into contact with water. This is particularly true in boat lifts and docks, where
lead screws for example can be entirely submerged in water for extended lengths of time. Boat lifts are one of the most important applications for lead screws, as a high load capacity is essential to be able to withstand the weight of the boat. Other applications include various moving components on the interior of a boat such as windows, adjustable television stands and seating adjustments.