Press |
|
Do you have any questions? Require materials? Current news releases and printable images are available for download here. Of course, we look forward to your call, email or fax! |
|
Press contactWould you like to be added to our media distribution list?igus® media digest |
实现极高动态和极低噪声运行的拖链4/5/2017
igus公司开发的E6.1拖链系列,适用于极耐磨损的应用需求,例如半导体无尘车间。与之前的E6系列一样,为了确保运行的减震和平稳,连接拖链侧板的是弹性元件,而不是孔销连接方式。因为链节的结构设计和其非常小的节距,可以将多边形效应降至最低,从而使拖链非常平滑地运行。其壁厚设计比E6更窄,在相同的内部尺寸下大约可节省30%的厚度。igus拖链系统总经理Harald Nehring表示:“这种设计原理还具有安静运行和极低振动的优点,噪声分贝只有32 dB(A)。因此E6.1拖链系列不仅可以应用在无尘室中,还非常适用于舞台技术或电视演播室。”同样,也适用于速度高达20米/秒的应用。从现在起,E6.1拖链系列提供四种不同的内高选择,内高在29毫米到62毫米之间。2017年春季,E6.1还会推出更大尺寸,内高为80毫米。 易于操作,快速装配 在E6.1所有尺寸的安装中,横杆都可以沿着内、外半径打开,从而实现快速填充。这样即使拖链已经安装在机器中,也能轻松地添加更多的电缆或软管。几乎所有的横杆都有定位刻度,便于精确布置分隔片位置。当内部高度需求是29毫米时,用户还可以选择订购横杆带旋转打开功能的拖链。这样操作起来更便捷,安装时间也更短。平滑的内腔设计,有效保护了内部电缆和管线,延长其使用寿命。 新闻联系: 王波 市场部经理 易格斯(上海)有限公司 浦东新区外高桥自贸区德堡路11号46号厂房 200131 上海 电话:+86 - 21 - 5130 3134 传真:+86 - 21 - 5130 3233 andywang@igus.com.cn www.igus.com.cn/press 关于易格斯: igus GmbH是国际领先的拖链系统和工程塑料滑动轴承制造商。该家族公司总部设在科隆,业务遍布35个国家或地区,全球员工约2,950人。2015年,igus面向运动应用的运动塑料达到5.52亿欧元的销售额。igus运营着业内最大的测试实验室和工程,根据客户需要提供创新产品和解决方案并快速交付。 "igus", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "energy chain", "energy chain systems", "flizz", "iglide", "iglidur", "igubal", "invis", "manus", "motion plastics", "pikchain", "readychain", "readycable", "speedigus", "triflex", "twisterchain", "plastics for longer life", "robolink", "xiros", "xirodur"和"vector"是igus® GmbH/科隆在德意志联邦共和国以及国际一些国家中受法律保护的商标。 |