Press |
|
Do you have any questions? Require materials? Current news releases and printable images are available for download here. Of course, we look forward to your call, email or fax! |
|
Press contactWould you like to be added to our media distribution list?igus® media digest |
可在-40℃下使用:25条拖链如何帮助飞机做好飞行准备9/25/2019
飞机除冰和清洗仍是一个需要人力作业的过程。为了缩短时间、降低延误率和成本,MSG Production AS公司推出了一体化全自动维护系统,来实现飞机除冰和清洗的自动化。这家挪威公司为其系统选用了极具性能优势的igus工程塑料产品:E2和E4系列拖链确保了可靠的电缆引导,igubal基座轴承则用于清洁喷嘴的安装。 飞机除冰工作成本高且耗时,其中多个步骤仍然需要人工干预。而且机场往往需要同时对多架飞机进行除冰,因此如何提高除冰效率成为了机场工作的一个瓶颈。这也是飞机清洗作业面临的难题。手动清洗波音737是一项需要花费十个小时才能完成的作业。所以,MSG Production AS公司开始着手解决这些难题,并首次开发出一款固定式的全自动维护系统,用于飞机的自动除冰和清洗。它可以将除冰时间缩短到7分钟,清洗时间缩短到20分钟。整个系统的主体由三个横梁构成,每个横梁上悬挂着两个伸缩臂和横杆。横杆和地板上都有一个喷嘴系统。飞机由电动牵引车牵引进入类似于自动洗车机的机库后,通过这款全自动维护系统进行清洗或除冰。由于整个系统需要在高湿度、化学腐蚀和寒冷的环境下可靠运行,因此制造商对系统部件提出了特殊的要求。而igus拖链可以安全可靠地引导软管和电缆,满足了开发人员对于拖链的特殊要求。 igus拖链让线缆排布更轻松 整个全自动维护系统使用了25条igus拖链:除了19条E4.1系列拖链外,还安装了6条2400系列拖链。这些拖链都由高性能工程塑料igumid G制成,可确保拖链不受水分和化学品腐蚀。即使工况温度低至-40℃,拖链系统也可以正常运行。而且这两款拖链都防尘和免润滑,非常适用于除冰和清洗设备。 igubal基座球轴承实现喷嘴的免润滑运动 除了使用igus拖链引导电缆外,MSG Production AS公司还使用了其他igus产品。例如,使用igubal基座轴承来确保喷嘴的平稳运行。它们被安装在地板和横杆上,需要长期暴露在化学品和水分中。因此,与运动塑料专家igus的所有其他产品一样,这些基座轴承都是免润滑、耐腐蚀、耐磨损且低摩擦的。igus产品的另一个优点是可以使用在线工具快速、便捷地计算轴承和拖链的使用寿命。使用寿命的预测是基于每年在占地3,800平方米的igus内部测试实验室里进行的超过12,000项摩擦测试和100亿次循环测试所获得的数据。因此,用户可以获得可靠的轴承、拖链和电缆的使用寿命预测。这有助于避免意外的停机时间。 想要了解MSG系统是如何工作的,可以访问:https://www.youtube.com/watch?v=WNJbExXVJTs&feature=youtu.be |