衛生的かつ静かな引き出し構造を実現
ドライリンNT-60伸縮型レール
3/26/2020

イグス株式会社(東京都墨田区)は、衛生的、軽量、洗浄可能なソリューションが求められる環境向けに伸縮型レール ドライリンNT-60を開発しました。スライド部には高性能樹脂イグリデュール材質を使用しているため、無潤滑・メンテナンスフリーで軽量かつ静音な動作を実現します。

伸縮型レールは小さなスペースで物体を動かすことができるため、あらゆる場所で使用されています。この度イグスは、高荷重用で軽量かつ無潤滑なソリューションとして、ドライリンNT伸縮型レールシリーズを拡充しました。新しいドライリンNT-60は、幅60mm、高さ24mm、長さは用途に合わせて最大2,000mmまで無段階で自由に拡張ができます。本製品には硬質アルマイト処理アルミニウム製レールおよび高性能樹脂イグリデュールJ製スライドパーツを採用しています。イグリデュール材質には固体潤滑剤が配合されており、静音かつスムーズな動作が可能なだけでなく、グリスが不要なためレールに汚れや埃が付着せずメンテナンスフリーで使用でき、長寿命を実現します。簡単かつスピーディに高圧・薬品洗浄できるため、医療現場や実験施設などでご使用いただけます。

ドライリンNT-60は、曲げ応力を受ける部分がアルミニウム製のため優れた剛性を備えています。イグス試験施設で行った引き出し試験で、400mm拡張した2本のドライリンNT-60がハンドル付近で最大180Nの静荷重に耐えられることが実証されました。引き出しのように2本を水平に取り付けたり、個々に又は平行に取り付けたりすることも可能です。耐食性も備えており、屋内・屋外両方の用途にも対応しています。


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302