チェーンフレックスPROFINETケーブル CF898.061.FC10/28/2021

イグス(本社ドイツ)は、生産現場での迅速なケーブル加工のために、新しいチェーンフレックスPROFINETケーブル CF898.061.FCを開発しました。
この新しいPROFINETケーブルにはFastConnect技術が採用されており、わずか数ステップで簡単にケーブル被覆を剥ぎ取ることができ、ハーネス作業時間を最大46%短縮可能です。
また、イグスの他の可動ケーブル製品と同様に、エナジーチェーン ケーブル保護管内での可動用途において長寿命を実証済みで、最大36ヶ月の無償交換保証付きです。

世界で最も普及しているイーサネットベースの産業用ネットワークであるPROFINETにより、大容量のデータでもイーサネットプロトコルに基づいて最大100Mbit/sで伝送することができます。
そしてPROFINETケーブルは、工作機械や包装機械、マテリアルハンドリングの業界でRJ45コネクタと組み合わせてよく使用されています。
この度イグスは、コネクタを迅速に取り付けるため、耐屈曲性の高いチェーンフレックスPROFINETケーブル用のFastConnect技術を開発しました。
この技術を採用したチェーンフレックスCF898.061.FCは、わずか数ステップで加工してコネクタを取り付けることが可能です。


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302