Press |
|
Do you have any questions? Require materials? Current news releases and printable images are available for download here. Of course, we look forward to your call, email or fax! |
|
Press contactWould you like to be added to our media distribution list?igus® media digest |
兼顾低成本与耐用性:igus装配电缆还推出了经济型8/11/2016
在全球14个国家根据24个制造商标准生产新的装配电缆并选配原装接头 运动塑料专家igus推出的“readycable”表示装配电缆,包含4,000多种预装配电缆选择,这些都是基于所有主要制造商的标准。igus现在用chainflex M高柔性电缆进一步扩展了驱动电缆范围系列,并提供了多种预装配选项,如指定长度(精确到厘米),并包括接头。这种经济型的电缆系列适合中等负载的运动应用,最高可完成五百万次往返运动,价格便宜约60%。 可直接连接的电缆在交付后即可使用——这是生产装配电缆的简单原则,按所需长度1件起订,无最小订购量,igus也不收取任何附加费用。igus在超过4,000种chainflex预装配高柔性电缆系列的基础上增加了低成本的chainflex M高柔性电缆并匹配了接头,符合24个制造商的标准。该系列比igus其他目录电缆便宜约60%,同时也拥有36个月的使用寿命保证。igus装配拖链和装配电缆主管Christian Stremlau表示:“预装配的chainflex M高柔性电缆提供高性价比的解决方案,可完美适用于重载循环以及速度和加速度方面有中等要求的应用。用户现在可在更多产品中选择更适合自己应用且最便宜的电缆。”电缆大部分装配工作都是通过机器完成的,因此可实现最高的品质标准。这样可提升装配电缆的生产速度,并增强它在应用流程中的可靠性。使用新的装配电缆查找器2.0 ( www.igus.eu/readycable-finder)可轻松找到所需的合适产品。客户可在此选择合适的驱动电缆,指定所需的长度,然后订购。输入电动机制造商的零件号就能立即显示出igus与之匹配的电缆,配置更加简单。 全球化的装配电缆——36个月的质保承诺 为确保快速、有针对性的交付,igus已大幅提升了其在北美、亚洲和欧洲的生产和装配能力。由此,客户可从igus全球14个仓库和装配中心快速准确的获得满足其应用需求的产品。与所有电缆一样,igus也为chainflex M高柔性电缆产品系列的装配电缆提供36个月的使用寿命保证。这意味着,在持续运动应用中多达500万次往返运动的功能可靠性得以保障。与常规产品一样,电缆在24小时内发货,精确到厘米,无剪切费用,1件起订,无任何最小订购量附加费。 |