Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270
US(EN)

Training Quietly with igus® Bearings

"Thanks to iglide® plastic bearings and igubal® rod end bearings, the company was able to save at least $15,000 U.S. a year in production costs and considerably reduce assembly times."

Problem 1:

Pivot bearings were necessary for the chain tensioners on all training equipment. The machine has a drive train that consists of top and bottom pedal cranks for arms and legs. The pedal cranks are linked and drive a resistance load via a roller chain. So that the alignment between the teeth on the sprocket is ensured, the axial position was adjusted and varied from machine to machine. This increased the assembly time and made work complicated for service engineers. When the teeth wear down, this caused a dynamically varying chain line during operation, which resulted in excessive noise and the possibility of the chain jumping out.
Shop iglide® L280 bearings

Solution:

Using iglide® L280 bearings in the chain tensioner enables both the axial and rotary motion of the roller. This prevents the need for time-consuming alignment during assembly. The result is faster assembly, easier servicing and no more chains jumping out.

Problem 2:

Furthermore, 4 iglide® L280 plain bearings are used on the training equipment to adjust the crank arms on the part of the appliance for the upper body. The earlier design required a high degree of precision, which could not be achieved mechanically. The leveling was therefore done by hand in order to level the crank arm clips with the corresponding dovetail slots. Every little bend or misalignment due to a knock affected the performance of the adjusting mechanism. Maintenance was extremely difficult and the adjusting slots on the back of the crank reduced the strength of the crank arms, which often led to breakdowns during high load applications.

Solution:

As a solution, parallel guide rods were designed, which allow a torsion-resistant linear motion. iglide® L280 bearings were used for each rod in pairs with a gap between them in order to enable a linear motion with low friction, high endurance and minimal room between bearing and rod. Stiffness is achieved due to the low installation height, noise is minimized and the steel rods are less prone to damage. All crank arms can be connected with each cam mechanically, meaning there is no more need for manual adjustment.

Problem 3:

A third application on a totally new piece of training equipment contained a crank arm with a dynamically variable length for use on a training bike. It varies during a cycle depending on the user's feet position by means of a cam and guide roller. An earlier prototype optimized an expensive, customized series roller plain bearing, but this solution repeatedly failed due to the constant misalignment, deflection and noise level. The change in size of the design proved too expensive. The solution was to find an appropriately durable, rigid and tool-free design.

Solution:

A design was developed consisting of a crank arm bearing with a set of iglide® L280 ball bearings, which slides along on a pair of parallel steel rods. This also contains an igubal® ball bearing, which activates a steel pin that is fastened to the crank arm bearing. The crank arms are now sufficiently rigid and a misalignment due to inaccuracies in the bike frame and the sub assembly, as well as stress caused by the user, is compensated without exerting extreme loads on the machine and crank mechanism, as was the case on earlier prototypes.

Discuss your project with a bearings expert

Whether you're interested in turnkey, fully assembled solutions or looking to build your own customizable project, learn more about how igus® can assist you with a solution based on your specific application and requirements. Contact us via the form below or call us at (800) 521-2747 to discuss your project today!

Contact an igus® expert now



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302