Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270
US(EN)

Pre-assembled cable carrier systems for laser cutting machines

Dynamics and precision

The advantages of laser cutting technology is its lightning speed and flexibility. Even small orders, different plate thicknesses and band widths can be cost-effectively processed.

One universal laser cutting system for plate formats of 9.8 x 4.9 ft has been on the market since 2001. The maximum axis acceleration is 98.4 ft/s² or 492.1 ft/min, which is equivalent to 3 g.

High demands on the supplier

Pre-assembled readychain® cable carrier systems from igus® were chosen for the energy supply, for which the manufacturer wanted to procure everything from one source. By working exclusively with igus® on this project, the company drastically reduced the number of suppliers they had to work with.

Due to the extremely high dynamics involved in this demanding application, the cable carrier had to be stable, rugged and not too heavy. The energy chain experiences very high cross accelerations, especially on the Y axis.

The pre-harnessed cable carrier is filled with a multitude of control and drive cables. The motor cable for the Y axis assumes the most significance, as it is the cable with the largest diameter.
cable carrier for laser cutting machine The laser cutting machine in action

Delivered right on time

igus® is committed to keeping a certain quantity of pre-assembled readychain® cable carrier systems ready to deliver to the laser cutting facility within a set period of time. For this reason, igus® can respond flexibly to the factory’s requirements. The cable carrier system is delivered directly to the machine exactly when it is needed. This system shortens installation times and frees up storage space on-site.
Pre-harnessed cable carriers Simple packaging that can be disposed of easily

More product information

More application examples from different industries



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302