Inquiry / Contact
igus® inc.

PO BOX 14349

East Providence

RI 02914

+1 800 521 2747
+1 401 438 7270
US(EN)

Cable carrier suitable for long travels and hot metal chips

Horizontal guide system for CNC-turning machine

Tornos Gurutzpe S.A. has been in business for 52 years and has delivered well over 5,000 machines over that period. Specializing in large-capacity lathes, the company sells to customers in the United States, Europe, India and elsewhere. It supplies turbine parts for power plants, drill pipes for oil production, laminated and hydraulic cylinders. Its best-known customers include suppliers of Spanish oil company Repsol, and railroad companies SNCF (France) and RENFE (Spain), as well as elevator companies including ThyssenKrupp Elevators and U.S. company Halliburton.

The company’s latest horizontal CNC-turning machine, the A-2000 4G CNC, is designed to be reliable, resilient and efficient: top requirements for lathe buyers all over the world. It required a cable-carrier solution that was suitable for unsupported long travels and hot metal chips.

About 30 machines leave the Gurutzpe factory each year. The company’s focus is on the durability of each machine, according to sales manager Oscar Anitua, "Even decades-old machines made by us are still operated by our customers."

An initial prototype of the new A-2000 4G CNC was delivered to a customer in the wind-energy sector equipped with two horizontal Guidelok systems running side-by-side over a distance of 44 feet.

Plastic more resistant than heavy steel

Joaquín Orbegozo, head of electrical engineering at Gurutzpe, is convinced of the advantages of Guidelok, "The cable carriers are rugged, rigid and reliable."

He explains this to customers, "Sometimes one says, I would have liked this or that machine, but with a metal cable carrier.” Then Orbegozo explains the benefits of lighter, robust plastic cable carriers, demonstrating that they can easily tolerate the weight of a grown man.

If another customer has a concern that, during the machining process, hot metal chips could eat through the plastic, Orbegozo takes a soldering iron and presses it onto the cable carrier in a few different places, "When customers see that this cannot damage the cable carrier, they are convinced.”
Guidelok horizontal guiding system Guidelok is designed to stop metal chips causing abrasion and wear in long travel cable carrier applications.

Longer travels for CNC-turning machines

Gurutzpe specializes in special turning machine solutions for customers with specific requirements. Currently only two manufacturers worldwide offer prismatic-turning machines, for example. Gurutzpe also makes guide machines equipped with fixed or hydraulic steady rests and offering a great degree of flexibility.

The company has seen market demand increase when it comes to very large, long travel CNC-turning machines. "Gurutzpe has already built turning machines 66 feet long," says Anitua.

Safe cable guidance shouldn’t be an issue for these applications, since igus’ Guidelok cable carrier systems can cope with distances up to 164 feet.
cable carrier for heavy steel chain Machine-tool manufacturer replaces a heavy steel chain with Guidelok

More solutions for long-travel applications here

Additional application examples from different industries



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "kineKIT", "manus", "motion plastics", "pikchain", "plastics for longer life", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsibushi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention in this website. The products offered by igus® are those of igus® GmbH

igus inc headquarters is located at 257 Ferris Ave, Rumford, RI 02916. igus enjoyneering center is located at 2055 Franklin Rd, Bloomfield Twp, MI 48302