Change Language :

The ”Virtu“ large-format printer can be used to print almost anything: sheetmetal, foils, textiles, wood, glass, and, of course, also paper in widths up3,5 metres. To do this, a print head moves at a speed of up to 3 metres persecond over the medium to be printed. Since even the slightest vibration wouldaffect the printed image, an energy supply system that runs as smoothly aspossible had to be found. Here the decision went to the low-vibration andextremely quiet igus® E6 energy chain cable carrier.
Spühl AG, Stephan Keller,
Wittenbach, Switzerland
More on applied products here
More applications from different sectors