Change Language :
The company developed a mechanism with which anyone can lift a heavy outboard motor up and down onto a sailing boat trestle without straining, whilst at the same time being able to watch shipping traffic in front of the bow. Various solutions were tested but were too expensive, did not turn correctly or were much too loud. The company then wanted to build an electrically operated vertical lift.
The company opted for wheels (iglide® J plain bearings), that rotate as soon as they are exposed to the torque pressure from the offset motor, in order to prevent friction between the wheel and the aluminum rails. By using iglide® J, the wheel assemblies were able to rotate freely without making a noise. "Install bearings from igus®. The result was spectacular ... anyone for sailing?" said the company owner.

Whether you're interested in turnkey, fully assembled solutions or looking to build your own customizable project, learn more about how igus® can assist you with a solution based on your specific application and requirements. Contact us via the form below or call us at (800) 521-2747 to discuss your project today!