Change Language :
Intelligent products announce maintenance date ahead of time and can be integrated into a process of predictive maintenance.



Attached to different crossbars, igus® isense EC. L-modules in combination with the icom communication module are able to assess the current condition of an e-chain®. The acceleration and temperature sensor EC. M(otion) on the one hand and the abrasion sensor EC. W(ear) on the other hand collect data continuously and send it to the "open source solution" (icom). Among other things, icom collects and evaluates data from the EC. L modules so that replacement or repair requirements are predicted and production plants can run smoothly and efficiently.

isense EC.P – P(ush/Pull) – formerly the igus® PPDS
Used to monitor the push/pull forces of igus®e-chains® over long travel distances. EC. P is a combination of load cell (force monitoring, pull/push force monitoring) and the isense EC. P (PPDS-Box). The load cell is either build into the connecting element of the e-chain® or integratedinto the floating moving end.
isense EC.B – B(reakage) – formerly igus® EMA
Determines breakage of a link caused by accidents or vandalism. EC.B includes a polymer wire in special separators and a sensor unit. The information from the sensor unit can either be analyzed by the isense EC. P (PPDS) or the sensor unit can be directly connected to the customer‘s system on site.

NEW: isense EC.RC
Monitoring the operating status of e-chains®, especially in guide troughs where long travels are involved. Sensors measure and check the position of the energy chain. so the machine won't continue operating when mechanical faults occur and a total loss of the chain or an electrical shutdown (for example, due to cable damage) can be prevented.

Used to detect the wear limit of drylin® linear units.A plastic element that has an integratedsensor which signals the need for replacement ahead of time. Can be fitted subsequently.

Mounted in a milled slot below the sliding elements, the PRT. W sensor measures wear and tear and can indicate the required replacement promptly via the icom communication module, preventing cable failure.