Change Language :
Our flexible chainflex cables generally come with a guarantee of up to 4 years, as are our many new products this year. We would like to present extensive additions to the drive technology range. You will also find innovations from the product range for top drive applications and for applications in very dry environments.

... 12 additional months for more safety
The unique chainflex guarantee has been extended by another 12 months and is now valid for 4 years! Numerous tests in the 3,800m² test laboratory make such a guarantee possible!

... for the e-chain® and the cable tray
UL-listed flexible motor and control supply cables for use in the e-chain and the cable tray. These listed motor and control cables are ideal for continuous movement and for a seamless transition from the chain to the platform.

... operational safety in the onshore and offshore sector
The CFSPECIAL.572 has been added to the product range for suspended top drive applications, including DNV approval for use in the maritime sector.

... flexible cables with PVC outer jacket
Our new PVC cables are the right choice for oil-free applications. Typical sectors include woodworking, packaging and material handling.

... even more safety for cleanrooms
Increase in the guaranteed service life of CFCLEAN cable elements to 40 million double strokes and simultaneous increase in current-carrying capacity.

... operational safety guaranteed and confirmed worldwide
chainflex dispenses with PTFE! The new logo confirms the elimination of PTFE in igus chainflex cables. If a general ban is announced, no chainflex cables will have to be disposed of or replaced and can continue to be used worldwide without any concerns.

... tested in the chainflex® laboratory and with a guarantee
Six cable series with new cross sections were added to the chainflex product range. Our cables come with the unique chainflex guarantee and have been tested in our own test laboratory.

... resistant thanks to the TPE outer jacket
With the high-end motor cable series CF38, installation space can be saved and at the same time low temperatures down to -35°C can be withstood. With the new cross sections, we are expanding the CF38 family and at the same time replacing the discontinued models of the CF35.UL.

... thanks to TPE high-end single-core cable
The new CF340.100.01 is an addition to the CF340 single-core family and, thanks to the robust TPE outer jacket, is ideal for small installation spaces in the energy chain and long travels.

... specifically developed for dry environments
The CF211 encoder cable series has been expanded for the SINAMICS V90 drive system. Robustness for dry environments is guaranteed thanks to the PVC jacket. The new chainflex CF211.030 is available from stock sold by the metre or harnessed ready for connection.

... for CAN bus and Ethernet up to CAT7
The service life of the CFROBOT8.PLUS has been increased by the larger torsion angle of up to +/- 360°/m and solves problems in tight installation spaces.

... CF98.PLUS and CF99.PLUS guaranteed with 100,000,000 double strokes
The new CF98.PLUS and CF99.PLUS control cables achieve the longest durability with 100,000,000 double strokes or a bending factor of 3xd.

... extended for the ctrlX DRIVE system from Bosch Rexroth
Suitable for drives of the MS2N series from Bosch Rexroth, you reduce costs by 50% and receive the usual service life guarantee.

... for SINAMICS 210 drives ...
With the new PVC hybrid cable, we are adding to the CF220.UL.H cable series and thus offer even more variety. Thanks to the high-quality PVC outer jacket, you can save 15.3% of costs.

... now with DNV approval
With the new DNV approval, the CFSPECIAL.5XX series is the perfect solution for offshore drill rig applications.