igubal® pillow block bearings with clip-on design

igubal CL pillow block bearings
Tech up
  • 30% greater tensile strength thanks to optimised housing (bio-mechanic design)
  • Can be combined with all spherical ball materials for a wide range of requirements
  • Faster delivery times
  • More even movement of the spherical ball in the housing
Cost down
  • The cost is about 10% less than that of the overmoulded version with the same spherical ball material
  • Further savings potential with low-cost spherical ball materials
  • One-to-one interchangeability with the overmoulded version because the dimensions are the same
  • Depending on the application, the alternative spherical ball material can extend service life
Proof
  • Tested in the laboratory
Sustainability
  • Environmentally friendly, as [Link pagenr="2323" title="no additional lubricants are necessary" parameter="#section_4 "]
  • Good coefficient of wear and therefore a long service life
  • igus supports the circular economy of plastics and is investing in chemical recycling

Short news presentation for the igubal KSTM-xx-CL pillow block bearing

Pillow block bearing consulting

What is iglide?

Online seminars