Change Language :


1.1 igus®' iglide'® N54 plastic bushings are made out of 54 percent raw, renewable materials.
In the words of Kermit the Frog, “It ain't easy being green.” And while he might be just a Muppet, Kermit has a point – these days, many companies are working hard to reduce their carbon footprint on the environment.
However, becoming a more environmentally friendly operation does not happen overnight. It is usually a culmination of changes that take place over time, in a number of different areas. So, what small change can you make to help this cause? While it might sound insignificant, using dry-running plastic bushings can greatly decrease any negative effects on the environment.
Here are four reasons to use environmentally friendly plastic bushings:

The heavier a material is, the more energy it needs to stay in motion. Bronze bearings need a lot of energy, while plastic bushings need much less.
Useful links