Change Language :

TPE motor cable with new insulation material for improved temperature stability with higher UL temperature

... reduce costs & increase service life
In the crane and material handling sector, installations are increasingly getting bigger and working at an ever-higher dynamics around the clock. This means, in addition to the ever-higher demand for energy, there are rising requirements on the components used, which have to withstand ever-increasing loads all 365 days of the year. The new motor cables can be used in indoor and outdoor applications due to the special conductor structure as well as the combination of the materials used.
There they are already in use in more than 10,000 port facilities worldwide and have therefore proven themselves in practice and under harsh application conditions. The fields of application include ship-to-shore cranes, bulk cargo handling cranes, RTGs, RMGs, Goliath cranes, spreaders, reach stackers, etc.